SANTA ROSA, Calif., November 12, 2019
Keysight Technologies, Inc. (NYSE: KEYS), a leading technology company that helps enterprises, service providers and governments accelerate innovation to connect and secure the world, today announced the i3070 Series 6 In-Circuit Test (ICT) suite of solutions which enables electronics manufacturers to improve test throughput and the operational efficiency of their printed circuit board assembly (PCBA) manufacturing.
Electronics manufacturers for the 5G, internet of things (IoT), and the automotive and energy industries are faced with a highly complex, connected global manufacturing environment. As manufacturing operations evolve, they need test systems that can provide high throughput as well as consistent and repeatable results to leverage the advantages of a "smart factory" environment including Industry 4.0.
Keysight 's i3070 Series 6 ICT supports a wide range of PCBA sizes for applications including IoT and 5G, as well as automotive and energy. The i3070 features a unique design that delivers the shortest signal path between measurement circuitry and devices under test to minimize undesired effects from parasitic capacitance, improve immunity to crosstalk, and eliminate stray signal coupling effects, delivering consistent and repeatable measurements.
Keysight 's i3070 Series 6 ICT offers customers:
"Manufacturing of printed circuit assemblies is a global operation that has recently experienced shifts to new locales due to macro-economic realities. It is crucial that in-circuit test platforms provide cross-geographic flexibility, where a test program written on one system can be quickly transported to another system that may be continents away," said Christopher Cain, vice president and general manager for Keysight 's Electronic Industrial Products. "The new i3070 Series 6 in-circuit test platform provides transportable test capabilities and adds advanced Industry 4.0 technology to deliver high yield, fast throughput and best-in-class operational efficiency for our top-tier printed circuit assembly manufacturing customers."
About Keysight Technologies
Keysight Technologies, Inc. (NYSE: KEYS) is a leading technology company that helps enterprises, service providers, and governments accelerate innovation to connect and secure the world. Keysight's solutions optimize networks and bring electronic products to market faster and at a lower cost with offerings from design simulation, to prototype validation, to manufacturing test, to optimization in networks and cloud environments. Customers span the worldwide communications ecosystem, aerospace and defense, automotive, energy, semiconductor and general electronics end markets. Keysight generated revenues of $3.9B in fiscal year 2018. More information is available at www.keysight.com.
# # #
Additional information about Keysight Technologies is available in the newsroom at https://www.keysight.com/go/news and on Facebook, LinkedIn, Twitter and YouTube.
Additional Information
Images of Keysight 's i3070 Series 6 In-Circuit Test family are available at https://www.keysight.com/find/series6-images.
Keysight Contact:
Geri Lynne LaCombe, Americas/Europe
+1 303 662 4748
geri_lacombe@keysight.com
Fusako Dohi, Asia
+81 42 660-2162
fusako_dohi@keysight.com