SANTA ROSA, Calif., May 14, 2019
Keysight Technologies, Inc. (NYSE: KEYS), a leading technology company that helps enterprises, service providers and governments accelerate innovation to connect and secure the world, announced the optional S93070xB Modulation Distortion application for the company's PNA-X Vector Network Analyzer, which delivers a wide system dynamic range resulting in the lowest possible residual error vector magnitude (EVM) on the market today.
Traditional test setups, especially for 5G power amplifiers and beamformer integrated circuit design, verification and production, are complex and can introduce a wide range of sources for potential errors. These include mismatch and cable loss, which compromise signal fidelity and reduce the accuracy and repeatability of measurements.
The new S93070xB Modulation Distortion application, which is fully integrated with Keysight's PNA-X Vector Network Analyzer, enables designers to accurately, repeatably and quickly characterize the behavior of a device under modulated wideband signal stimulus. It leverages state of the art calibration for the best accuracy, offers single connection and single touch for existing vector network analyzer measurements, and provides the lowest possible residual EVM available in the market today.
"Engineers need to simplify their test setups to perform accurate, repeatable measurements they can trust," stated Joe Rickert, vice president of high frequency measurement R&D, at Keysight Technologies. "Integrating modulation distortion on the PNA allows engineers to isolate and measure key performance parameters of their design, reduce complexity of test environments and eliminate potential sources of error. This provides them with the confidence that their measurement results are reliable and consistent."
Keysight's new S93070xB Modulation Distortion application offers the following key features to help customers overcome wideband measurement challenges, as well as easily reproduce and speed time of measurements:
Images are available at https://about.keysight.com/en/newsroom/images/modulation-distortion/
About Keysight Technologies
Keysight Technologies, Inc. (NYSE: KEYS) is a leading technology company that helps enterprises, service providers and governments accelerate innovation to connect and secure the world. Keysight's solutions optimize networks and bring electronic products to market faster and at a lower cost with offerings from design simulation, to prototype validation, to manufacturing test, to optimization in networks and cloud environments. Customers span the worldwide communications ecosystem, aerospace and defense, automotive, energy, semiconductor and general electronics end markets. Keysight generated revenues of $3.9B in fiscal year 2018. More information is available at www.keysight.com.
# # #
Additional information about Keysight Technologies is available in the newsroom at https://www.keysight.com/go/news, and on Facebook, LinkedIn, Twitter and YouTube.
Contact:
Geri Lynne LaCombe, Americas/Europe
+1 303 662 4748
geri_lacombe@keysight.com
Fusako Dohi, Asia
+81 42 660-2162
fusako_dohi@keysight.com