SANTA ROSA, Calif., February 19, 2019
Keysight Technologies, Inc. (NYSE: KEYS), a leading technology company that helps enterprises, service providers and governments accelerate innovation to connect and secure the world, today launched the first dual-channel microwave signal generators that support up to 44 gigahertz (GHz) signals and 2 GHz radio frequency (RF) modulation bandwidth in a single instrument.
Keysight's new VXG microwave signal generators address the most demanding wideband millimeter wave (mmWave) applications for 5G and satellite communications by decreasing test set-up complexity and reducing path losses introduced in over-the-air (OTA) test environments.
Many 5G New Radio (NR) deployments leverage wider channel bandwidths and active antenna arrays operating in mmWave frequency spectrum to support multiple-input and multiple-output (MIMO), as well as beamforming technologies. 3GPP mandated conformance testing of components, and other wireless network equipment aimed for deployment in mmWave frequencies, need to be performed in radiated OTA test environments.
Keysight's new VXG microwave signal generators support the next frontier of cellular technology with the following key benefits:
"We are excited to introduce the world's first dual-channel 44 GHz microwave signal generator with 2 GHz bandwidth, in both benchtop and modular form factors," said Joe Rickert, Keysight Vice President, High Frequency Measurement R&D. "The VXG's low phase noise, high output power, excellent modulation, and distortion performance make it an ideal signal generator for a wide breadth of applications in wireless communications, for commercial and aerospace defense industries."
Keysight's VXG signal generators offer designers and manufacturers of wireless equipment a wide range of advanced features, including:
Keysight's 5G waveform generation and analysis testbed solution leverages the VXG microwave signal generator's enhanced capabilities for 5G development teams to efficiently validate new designs across both frequency range 1 (FR1) and frequency range 2 (FR2) as defined by 3GPP. The testbed solution uniquely addresses the challenges of 5G NR conformance test and enables Keysight to quickly integrate new technology into market-ready solutions that enable customers to move faster and achieve first-to-market goals.
Additional Information
About Keysight Technologies
Keysight Technologies, Inc. (NYSE: KEYS) is a leading technology company that helps enterprises, service providers, and governments accelerate innovation to connect and secure the world. Keysight's solutions optimize networks and bring electronic products to market faster and at a lower cost with offerings from design simulation, to prototype validation, to manufacturing test, to optimization in networks and cloud environments. Customers span the worldwide communications ecosystem, aerospace and defense, automotive, energy, semiconductor and general electronics end markets. Keysight generated revenues of $3.9B in fiscal year 2018. More information is available at www.keysight.com.
# # #
Additional information about Keysight Technologies is available in the newsroom at https://www.keysight.com/go/news, and on Facebook, Google+, LinkedIn, Twitter and YouTube.
Contact:
Geri Lynne LaCombe, Americas/Europe
+1 303 662 4748
geri.lacombe@keysight.com
Fusako Dohi, Asia
+81 42 660-2162
fusako_dohi@keysight.com