SANTA ROSA, Calif., January 29, 2019
Keysight Technologies, Inc. (NYSE: KEYS), a leading technology company that helps enterprises, service providers, and governments accelerate innovation to connect and secure the world, announced a comprehensive transmitter (Tx) and receiver (Rx) testing solution providing the speed and margins needed to meet the Peripheral Component Interconnect or PCI Express® 5.0 Technology (PCIe® Gen5) standard.
With many 5G wireless devices reported to launch in 2019, the computer/server industry is actively working to upgrade and enhance network speed with advanced technologies such as 400G Ethernet. PCI Express 5.0 technology is required for computer servers to support the bandwidth of 400G networks, as it is the only significant input/output (I/O) interconnect that has the throughput necessary to support the 400G interface.
Designing integrated circuits and systems utilizing this version of the PCIe standard presents significant engineering challenges for developers. Keysight's comprehensive PCIe 5.0 transmitter and receiver solution enables engineers with the tools necessary to achieve the speed and margins required to meet the standard, with upgradability for future investment protection.
"Data centers need to be upgraded to the next 400G speed rates for operators to offer new services, while preserving quality, meeting the ever-increasing data and storage demands, and minimizing costs," said Dr. Joachim Peerlings, vice president and general manager of Keysight's Networks and Data Centers. "Physical layer transmitter and receiver test tools capable of testing at 32GT/s enable designers to optimize their transmitter, receiver, and channel designs for maximum performance and reliability at the required increased data transfer rate."
The Keysight PCIe 5.0 receiver test solution enables the design and validation of circuits capable of tolerating significantly attenuated signals at 32 GT/s. PCIe 5.0 utilizes aggressive equalization techniques helping the receiver restore the quality of the transmitted signal, allowing for error-free recovery of the digital information from the PCIe Tx signal. Due to these high data transfer rates, PCIe 5.0 receivers must accept a heavily degraded signal resulting from the channel's high-frequency loss characteristics, resulting in unacceptable bit error ratios (BERs). To address this, Keysight has developed the M8040A High Performance 64Gbaud BERT, enabling physical layer characterization and compliance testing, to characterize receiver performance margins on the physical layer.
In addition, the increase in digital transmission speed and throughput introduce significant signal integrity challenges such as issues with connector crosstalk and receiver jitter sensitivity, driving the need for an accurate oscilloscope and receiver test solution. Keysight's Infiniium UXR-Series oscilloscope provides industry leading bandwidth and noise floor performance to maximize margins and meet the challenges presented by the PCIe 5.0 standard, with upgradeability to 110 GHz.
About Keysight Technologies
Keysight Technologies, Inc. (NYSE: KEYS) is a leading technology company that helps enterprises, service providers, and governments accelerate innovation to connect and secure the world. Keysight's solutions optimize networks and bring electronic products to market faster and at a lower cost with offerings from design simulation, to prototype validation, to manufacturing test, to optimization in networks and cloud environments. Customers span the worldwide communications ecosystem, aerospace and defense, automotive, energy, semiconductor, and general electronics end markets. Keysight generated revenues of $3.9B in fiscal year 2018. More information is available at www.keysight.com.
# # #
Additional information about Keysight Technologies is available in the newsroom at www.keysight.com/go/news, Keysight blog, and on Facebook, Google+, LinkedIn, Twitter and YouTube.
Contact:
Geri Lynne LaCombe, Americas/Europe
+1 303 662 4748
geri_lacombe@keysight.com
Fusako Dohi, Asia
+81 42 660-2162
fusako_dohi@keysight.com