302 Moved Temporarily

This document you requested has moved temporarily.

It's now at https://localhost:8955/main/header.jspx?curr_url=http://about.keysight.com/en/newsroom/backgrounders/33500B/index.shtml?cc=US&myAgilentEmail=&section=bd&lc=ger&cc=DE.

Understanding Keysight Technologies’ Trueform Waveform Generation Technology

March 3, 2014

  1. Introduction
  2. Comparison of Trueform Technology to PPC Generation Methods
  3. Comparison of Trueform Technology to DDS Generation Methods
  4. Improved Signal Integrity
  5. Generate the Exact Waveforms You Want
  6. Summary
  7. About Agilent Technologies
  8. Related Information

Introduction

Trueform waveform generation technology is an exclusive technology found in Keysight's 33600A and 33500B Series Trueform waveform generators. Trueform technology provides measurable advantages over Direct Digital Synthesis (DDS), the previous generation technology used in function/arbitrary waveform generators. These advantages include significantly lower waveform jitter for less test uncertainty and a true representation of the selected waveform, not an approximation. In this overview, we will introduce you to Trueform technology and compare Trueform to Point-Per-Clock (PPC) and DDS technology for waveform generation.

Comparison of Trueform Technology to PPC Generation Methods

Conceptually, the simplest way to gen­erate a waveform is to store its points in memory and then read those points out one after another and clock them into a data acquisition module (DAC). After the last point has been read, the generator jumps back to the first point again to begin the next cycle. This is sometimes called PPC generation.

Even though this method seems like the most intuitive way to create waveforms, it has two significant drawbacks. First, to change the waveform's frequency or sample rate, the clock frequency has to change, and making a good low-noise variable-frequency clock adds cost and complexity to the instrument. Second, since the step­wise output of the DAC is undesirable in most applications, complex analog filtering is needed to smooth the steps out. Because of its complexity and cost, this technology is used mainly in high-end waveform generators.

Comparison of Trueform Technology to DDS Generation Methods

DDS uses a fixed-frequency clock and a simpler filtering scheme, so it's less expensive than the PPC method. In DDS, a phase accumulator adds an increment to its output in every clock cycle, and the accumulator's output represents the phase of the waveform. The output frequency is proportional to the increment, so it's easy to change frequency even though the clock frequency is fixed. The output of the accumulator is converted from phase data into amplitude data typically by passing it through some type of look-up table.

The phase accumulator design allows DDS to use a fixed clock, but still execute waveforms at a perceived faster sample rate than the clock. So with DDS, not every individual point is being expressed in the resulting output waveform. In other words, DDS is not using every point in waveform memory, but it creates a really good approximation. But since it is an approximation, waveform data is changed in some way. DDS can skip and/or repeat aspects of the waveform in an unpredictable way. In best-case scenarios, this leads to added jitter; in worst-case scenarios, severe distortion can result. Small features in the waveform can be partly or completely skipped over.

Keysight's Trueform technology represents the next advancement in waveform generation technology. Trueform provides the best of both worlds. It gives you a predictable low-noise waveform with no skipped waveform points like PPC technology, but at the price point of DDS tech­nology. Trueform works by employing a patented virtual variable clock with advanced filtering techniques that track the sample rate of the waveform. In the following sections, we will look at some of the waveform generation advantages Trueform provides over DDS.

Improved Signal Integrity

One of the key advantages Trueform provides over DDS is overall better signal integrity. You can see the advantage in the frequency domain by comparing spectra and the time domain with a jitter measurement comparison. Figure 1 shows a frequency domain view of a 10 MHz sine wave generated using Trueform technology. Figure 2 shows the same frequency domain view of a 10 MHz sine wave generated with DDS technology.

Figure 1: Harmonics from Trueform technology using a 33500B Series Trueform waveform generator

Figure 1: Harmonics from Trueform technology using a 33500B Series Trueform waveform generator

Figure 2: Harmonics using a DDS-based generator

Figure 2: Harmonics using a DDS-based generator

Ideally, a sine wave would consist of the fundamental frequency with no harmonics, but in the real world this does not happen, so you want the harmonics to be as small as possible. In both Figures 2 and 3, in the upper right corner of the screen you can see how many dB the second harmonic is from the fundamental frequency. You can see the Trueform second harmonic is >5 dB lower than the DDS second harmonic. Also on the DDS figure, you can visibly see the fourth and fifth harmonics poking up from the noise floor. Finally in the DDS Figure 1 you can even see a non-harmonic spur between the fourth and fifth harmonic.

Figure 3: Jitter measurement on Trueform signal using a 33500B Series Trueform waveform generator

Figure 3: Jitter measurement on Trueform signal using a 33500B Series Trueform waveform generator

When we compare the two from a jitter measurement perspective, the Trueform advantage becomes even more pronounced. The following figures show a jitter measurement made on a 10 MHz pulse signal using a high-performance oscilloscope. The scope view is zoomed in on the rising edge of the pulse signal with the persistence setting of the scope turned on. The histogram function of the scope is used to measure the period jitter of the signals. The stan­dard deviation measurement in each figure is circled in red and represents the signal's RMS jitter. The Trueform pulse signal Jitter measurement is shown in Figure 3 and the DDS pulse signal jitter measurement is shown in Figure 4.

Figure 4: Jitter measurement on DDS signal using a DDS-based generator

Figure 4: Jitter measurement on DDS signal using a DDS-based generator

For the Figures 3 and 4, both the amplitude and time scales for the scope are the same. The Trueform pulse waveform has more than 10 times less jitter compared to the DDS pulse waveform.

The improved signal integrity Trueform offers over DDS means less uncer­tainty in your tests. This is especially true when you consider edge-based timing applications like generating a clock signal, trigger signal or commu­nication signal. The decreased jitter directly translates into less timing uncertainty in your test.

Generate the Exact Waveforms You Want

As we mentioned earlier, DDS uses a fixed clock and a phase accumulator so it cannot guarantee that every point or feature in a waveform will be played. The higher the frequency, the more gaps you will see in the output waveform compared to the ideal wave­form. Trueform, on the other hand, plays every waveform point regardless of the set frequency or sample rate. This becomes critical when you are dealing with a waveform that may have a small detail that is critical to the test you are performing.

As an example, we created an arbitrary waveform that consisted of a pulse with seven descending amplitude spikes on top of the pulse. The waveform was then loaded into a Trueform waveform generator and a DDS function/arbitrary waveform generator. First the waveform was played at a 50 kHz frequency on each generator. The result was captured on a scope, as shown in Figure 5. The yellow trace is the Trueform wave­form and the green trace is the DDS waveform.

Figure 5: Arbitrary waveform comparison at 50 kHz using a 33500B Series Trueform waveform generator

Figure 5: Arbitrary waveform comparison at 50 kHz using a 33500B Series Trueform waveform generator

In Figure 5 at 50 kHz, each generator was able to reproduce the waveform with seven spikes on top of the pulse. You can see that the Trueform spikes reached higher amplitude. In the Figure 6 scope screen shot, the waveforms were played again, but this time at 100 kHz. At 100 kHz, the Trueform waveform generator played all seven spikes and the DDS generator did not play any of the spikes. In the Figure 7 scope screen shot, the waveforms were played again, but the frequency was doubled again to 200 kHz.

Figure 6: Arbitrary waveform comparison at 100 MHz using a 33500B Series Trueform waveform generator

Figure 6: Arbitrary waveform comparison at 100 MHz using a 33500B Series Trueform waveform generator

Figure 7: Arbitrary waveform comparison at 200 kHz using a 33500B Series Trueform waveform generator

Figure 7: Arbitrary waveform comparison at 200 kHz using a 33500B Series Trueform waveform generator

At 200 kHz, once again, the Trueform waveform generator shows all seven spikes in the waveform. The DDS generator went from playing no spikes at 100 kHz to playing three spikes at 200 kHz. Notice that the three spikes played in the 200 kHz waveform do not match the correct time location of any of the seven spikes that are in the actual waveform points. These waveform examples demonstrate that when working with waveforms that have fine detail, DDS cannot be trusted.

Summary

DDS technology has been the standard technology in previous generation waveform generators, because it offered a lower-cost alternative to high-end PPC technology. The major drawbacks to using DDS technology to generate waveforms are poor signal quality, in the form of jitter and harmonic noise, and skipping waveform points so you do not get a true representation of the programmed waveform. Keysight's patented Trueform technology represents the next advancement in waveform generator technology by providing the performance of PPC at the price of DDS. This means you get low jitter on output waveforms and you get the waveform you want every time.

Keysight's Trueform technology blends the best of DDS and PPC architectures, giving you the benefits of both without the limitations of either. Trueform technology uses an exclusive digital sampling technique that delivers unmatched performance at the same low price you are accustomed to with DDS waveform generation.

The tables below highlights the revolutionary capabilities of Trueform technology.

Figure 8: 33600A Series 80 & 120 MHz TrueformWaveform Generators

Figure 8: 33600A Series 80 & 120 MHz Trueform waveform Generators

Figure 9: 33500B Series 20 & 30 MHz Trueform waveform generators

Figure 9: 33500B Series 20 & 30 MHz Trueform waveform generators

About Keysight Technologies

Keysight is a global electronic measurement technology and market leader helping to transform its customers' measurement experience through innovation in wireless, modular, and software solutions. Keysight provides electronic measurement instruments and systems and related software, software design tools and services used in the design, development, manufacture, installation, deployment and operation of electronic equipment. Information about Keysight is available at www.keysight.com.

 

RELATED INFORMATION

Press Release:

Agilent Technologies’ 80- and 120-MHz Trueform Waveform Generators Deliver Unrivaled Capabilities and Signal Accuracy (2014-Mar-03)

Agilent Technologies Introduces New Family of Waveform Generators with Unrivaled Signal Accuracy
(2012-August-21)

Photos:

www.keysight.com/find/33500B_images

www.keysight.com/find/33600A_images

Video:

www.keysight.com/find/33600A_video

Backgrounder:

www.keysight.com/find/33600A_backgrounder

Keysight Documents:

For more information, go to www.keysight.com/find/trueform and www.keysight.com/find/33600A

Contacts:

Janet Smith, Americas
+1 970 679 5397
janet_smith@keysight.com
Twitter: @JSmithKeysight

Sarah Calnan, Europe
+44 (118) 927 5101
sarah_calnan@keysight.com

Connie Wong, Asia
+852 3197-7818
connie-ky_wong@keysight.com

> More Press Releases
> More Backgrounders