Images for Press Release

Agilent Technologies Introduces Premier-Performance Network Analyzer for Active Device Test

The following product photos are available for use by the media, based on the Keysight Photography Use Policy.

The newly designed architecture for Agilent’s PNA-X transforms a traditional network analyzer onto a true RF measurement solution for amplifiers, converters and mixers.

Image 1: The newly designed architecture for Agilent’s PNA-X transforms a traditional network analyzer to a true RF measurement solution for amplifiers, converters and mixers.

Download JPG (1.10MB)

Download TIF (12.90MB)

Agilent’s PNA-X is the only 2-port network analyzer available with an internal second source.

Image 2: Agilent’s PNA-X is the only 2-port network analyzer available with an internal second source.

Download JPG (0.82MB)

Download TIF (11.46MB)

The PNA-X is the new standard in microwave network analysis.

Image 3: The PNA-X is the new standard in microwave network analysis.

Download JPG (0.57MB)

Download TIF (5.82MB)

 

Related Information
  Press Release:

Agilent Technologies Introduces Premier-Performance Network Analyzer for Active Device Test
(2007-February-01)

  Agilent Document:

Defining A New Generation of Network Analyzers

  Keysight Photography Use Policy:

We will permit use of Keysight photography available via this site as long as the use will not disparage Keysight nor imply endorsement by Keysight. The photography cannot be changed or manipulated in any way with the exception of resizing or cropping. By downloading our product photography you are indicating that you accept these terms. Any commercial use of these images must be approved by Keysight Technologies.

ALL IMAGES USED MUST INDICATE:
"Reproduced with Permission, Courtesy of Keysight Technologies, Inc."

  How do I download images:

To download files in Windows, use the right mouse button on the desired format (JPEG or TIFF) and choose 'Save Target As...'