Images for Press Release

Agilent Technologies Introduces FieldFox RF Analyzer, World's Most Integrated Handheld for Wireless Network Installation, Maintenance

The following product photos are available for use by the media, based on the Keysight Photography Use Policy.

Agilent's  FieldFox RF Analyzer is the world's most integrated handheld instrument for wireless network installation and maintenance (I&M).

Image 1:
Agilent's FieldFox RF Analyzer is the world's most integrated handheld instrument for wireless network installation and maintenance (I&M).

Download JPEG (0.8MB)

Download TIF (9.2MB)

FieldFox's Smith chart can be used to display impedance matching characteristics in cable and antenna systems.

Image 2:
FieldFox's Smith chart can be used to display impedance matching characteristics in cable and antenna systems.

Download JPEG (0.6MB)

Download TIF (5.9MB)

FieldFox meets tough environmental standards (MIL-PRF-28800F) and its water resistant chassis withstands wide temperature ranges and humid environments.

Image 3:
FieldFox meets tough environmental standards (MIL-PRF-28800F) and its water resistant chassis withstands wide temperature ranges and humid environments.

Download JPEG (0.8MB)

Download TIF (6.9MB)

Image 4:
The FieldFox RF Analyzer's built-in spectrum analyzer allows technicians to scan up to 6 GHz and detect interfering signals.

Download JPEG (0.4MB)

Download TIF (4.5MB)

The FieldFox RF Analyzer's built-in spectrum analyzer allows technicians to scan up to 6 GHz and detect interfering signals.

Image 5:
The FieldFox RF Analyzer's built-in spectrum analyzer allows technicians to scan up to 6 GHz and detect interfering signals.

Download JPEG (0.2MB)

Download TIF (1.2MB)

The FieldFox RF analyzer makes return loss and distance to fault measurements at the same time, allowing users to test overall system performance and quickly identify faults that cause degradation.

Image 6:
The FieldFox RF Analyzer makes return loss and distance to fault measurements at the same time, allowing users to test overall system performance and quickly identify faults that cause degradation.

Download JPEG (0.7MB)

Download TIF (8.2MB)

 

Related Information
  Press Release:

Agilent Technologies Introduces FieldFox RF Analyzer, World's Most Integrated Handheld for Wireless Network Installation, Maintenance
(2008-October-01)

  Agilent Document:

Addressing the Challenges and Needs of the Wireless Network Installation and Maintenance Market, www.agilent.com/find/fieldfox_backgrounder.

  Keysight Photography Use Policy:

We will permit use of Keysight photography available via this site as long as the use will not disparage Keysight nor imply endorsement by Keysight. The photography cannot be changed or manipulated in any way with the exception of resizing or cropping. By downloading our product photography you are indicating that you accept these terms. Any commercial use of these images must be approved by Keysight Technologies.

ALL IMAGES USED MUST INDICATE:
"Reproduced with Permission, Courtesy of Keysight Technologies, Inc."

  How do I download images:

To download files in Windows, use the right mouse button on the desired format (JPEG or TIFF) and choose 'Save Target As...'