Introducing Keysight's 2016 Advanced Low Frequency Noise Analyzer

  
  

The following product photos are available for use by the media, based on the Keysight Photography Use Policy.

The E4727A A-LFNA hardware consists of a PXIe chassis and several modules that may be used to connect to various device types.

Image 1:
The E4727A A-LFNA hardware consists of a PXIe chassis and several modules that may be used to connect to various device types.

Low-JPEG Download (0.2MB)

High-JPEG Download (0.5MB)

By slicing the noise data at one frequency, we may see the trend in drain current noise ("Sid") as a function of bias current.

Image 2:
By slicing the noise data at one frequency, we may see the trend in drain current noise ("Sid") as a function of bias current.

Low-JPEG Download (0.2MB)

High-JPEG Download (0.9MB)

Related Information

Keysight Photography Use Policy:

We will permit use of Keysight photography available via this site as long as the use will not disparage Keysight nor imply endorsement by Keysight. The photography cannot be changed or manipulated in any way with the exception of resizing or cropping. By downloading our product photography you are indicating that you accept these terms. Any commercial use of these images must be approved by Keysight Technologies.

ALL IMAGES USED MUST INDICATE:
"Reproduced with Permission, Courtesy of Keysight Technologies, Inc."

How do I download images:

To download files in Windows, use the right mouse button on the desired format (JPEG or TIFF) and choose 'Save Target As...'