The following product photos are available for use by the media, based on the Keysight Photography Use Policy.
Image 1:
The Agilent E4980AL precision LCR meter with three cost-effective frequency options offers the best price/performance and application breadth among basic LCR meters in the industry.
Low-JPEG Download (0.2MB)
High-JPEG Download (3.0MB)
Image 2:
The Agilent E4980AL precision LCR meter is used for component characterization and evaluation, and also in material measurement applications in research and development as well as education.
Low-JPEG Download (0.2MB)
High-JPEG Download (2.9MB)