Introducing MIPI M-PHY v3.0 Interface S-Parameter and Impedance Testing for Agilent's ENA Network Analyzer

  
  

The following product photos are available for use by the media, based on the Agilent Photography Use Policy.

Image 1:
Agilent MIPI D-PHY and M-PHY solution coverage. Tx/Rx Interface S-parameter and Impedance Tests are supported by the E5071C ENA Option TDR.

Low-PNG Download (0.3MB)

Image 2:
The ENA Option TDR provides a one-box solution for high-speed interconnect analysis, including impedance, S-parameters and eye diagrams.

Low-PNG Download (0.2MB)

Image 3:
The MOI and test package work with ENA Option TDR for efficient measurements according to the MIPI M-PHY conformance test suite.

Low-PNG Download (0.2MB)

Image 4:
Both S-parameter measurement in the frequency domain and impedance measurement in the time domain are required in the MIPI M-PHY conformance test suite.

Low-PNG Download (0.1MB)

Image 5:
Hot TDR is the TDR and return loss measurement under actual operating conditions (active devices in the power-on state). It’s easy to measure with the ENA Option TDR.

Low-PNG Download (0.1MB)

Related Information

Keysight Photography Use Policy:

We will permit use of Keysight photography available via this site as long as the use will not disparage Keysight nor imply endorsement by Keysight. The photography cannot be changed or manipulated in any way with the exception of resizing or cropping. By downloading our product photography you are indicating that you accept these terms. Any commercial use of these images must be approved by Keysight Technologies.

ALL IMAGES USED MUST INDICATE:
"Reproduced with Permission, Courtesy of Keysight Technologies, Inc."

How do I download images:

To download files in Windows, use the right mouse button on the desired format (JPEG or TIFF) and choose 'Save Target As...'