The following product photos are available for use by the media, based on the Keysight Photography Use Policy.
Image 1:
Agilent's FieldFox pulse measurements simplify radar field testing.
Low-JPEG Download (0.2MB)
High-JPEG Download (6.1MB)
Image 2:
Pulse measurements made with FieldFox are consistent with those of benchtop analyzers.
Low-JPEG Download (0.1MB)
Low-PNG Download (0.1MB)
Image 3:
Carrying precision into the field is the key driver behind Agilent's FieldFox analyzers.
Low-JPEG Download (0.4MB)
High-JPEG Download (0.6MB)