Agilent Technologies' FieldFox Handheld Combination Analyzers for Precision Radar Performance Validation

  
  

The following product photos are available for use by the media, based on the Keysight Photography Use Policy.

Agilent's FieldFox combo analyzers offer all functionality required to perform precision radar system RF and microwave performance validation in the field.

Image 1:
Agilent's FieldFox combo analyzers offer all functionality required to perform precision radar system RF and microwave performance validation in the field.

Low-JPEG Download (0.3MB)

Pulse measurement mode with the U202XXA peak power sensors automatically captures and characterizes pulses to 40 GHz.

Image 2:
Pulse measurement mode with the U202XXA peak power sensors automatically captures and characterizes pulses to 40 GHz.

Low-JPEG Download (0.3MB)

Using FieldFox analyzers, civil aviation authorities worldwide now have the ability to dramatically reduce their cost-of-test, while increasing the uptime of their mission critical systems. Photo courtesy of INDRA S.A.

Image 3:
Using FieldFox analyzers, civil aviation authorities worldwide now have the ability to dramatically reduce their cost-of-test, while increasing the uptime of their mission critical systems. Photo courtesy of INDRA S.A.

Low-JPEG Download (1.4MB)

High-JPEG Download (7.4MB)

FieldFox simplifies the task of accurately characterizing radar system LRUs (Line Replicable Units). Photo courtesy of INDRA S.A.

Image 4:
FieldFox simplifies the task of accurately characterizing radar system LRUs (Line Replicable Units). Photo courtesy of INDRA S.A.

Low-JPEG Download (0.6MB)

High-JPEG Download (5.9MB)

Related Information

Keysight Photography Use Policy:

We will permit use of Keysight photography available via this site as long as the use will not disparage Keysight nor imply endorsement by Keysight. The photography cannot be changed or manipulated in any way with the exception of resizing or cropping. By downloading our product photography you are indicating that you accept these terms. Any commercial use of these images must be approved by Keysight Technologies.

ALL IMAGES USED MUST INDICATE:
"Reproduced with Permission, Courtesy of Keysight Technologies, Inc."

How do I download images:

To download files in Windows, use the right mouse button on the desired format (JPEG or TIFF) and choose 'Save Target As...'