The following product photos are available for use by the media, based on the Keysight Photography Use Policy.
Image 1:
Agilent’s new LTE-Advanced X-Series measurement application measures cumulative ACLR for non-contiguous carrier aggregation to ensure the RF requirement within the sub-block gap is within specification.
Low-JPEG Download (0.7MB)
Image 2:
Base station operating band unwanted emissions for non-contiguous carrier aggregation with a special aggregated mask takes into account contribution from each sub-block.
Low-JPEG Download (0.7MB)
Image 3:
Up to five component carriers can be displayed on the same screen to ensure the transmitted signal quality stays within the 3GPP requirement.
Low-JPEG Download (0.5MB)
Image 4:
The channel power of each component carrier or total power across the aggregated bandwidth can be measured to ensure accurate transmitter output power.
Low-JPEG Download (0.5MB)