The following product photos are available for use by the media, based on the Keysight Photography Use Policy.
Image 1:
The Agilent M9037A PXIe controller showing the various front panel interface connections.
Low-JPEG Download (0.2MB)
High-JPEG Download (2.2MB)
Image 2:
The Agilent M9037A PXIe controller, showing easy removal of the 240GB SSD.
Low-JPEG Download (0.3MB)
High-JPEG Download (3.3MB)
Image 3:
M9037A high performance PXIe controller in a chassis with the M9393A PXIe performance vector signal analyzer.
Low-JPEG Download (0.2MB)
High-JPEG Download (6.0MB)