The following product photos are available for use by the media, based on the Keysight Photography Use Policy.
Image 1:
Infiniium’s industry-leading signal integrity looks even better in the new user interface.
Low-JPEG Download (0.2MB)
Image 2:
Real time eyes and jitter can now be displayed simultaneously.
Low-JPEG Download (0.1MB)
Image 3:
Amplitude modulation makes analyzing envelopes and bursts easy.
Low-JPEG Download (0.1MB)
Image 4:
InfiniiSim provides the most comprehensive waveform transformation in the industry.
Low-JPEG Download (0.1MB)
Image 5:
Now every signal can be displayed as a real time eye simultaneously with the new user interface.
Low-JPEG Download (0.6MB)
Image 6:
Display all the analysis charts at once for deep analysis.
Low-JPEG Download (0.1MB)
Image 7:
The user interface supports up to eight waveform areas and 16 grids on each area.
Low-JPEG Download (0.1MB)