The following product photos are available for use by the media, based on the Keysight Photography Use Policy.
Image 1:
The Agilent T150 provides superior nanomechanical characterization via a unique actuating transducer that produces tensile force (load on sample) via electromagnetic actuation combined with a precise capacitive gauge.
Low-JPEG Download (0.3MB)
Image 2:
Shown (black enclosure) is the installation of the Agilent T150 UTM at the world-renowned Institute for Frontier Materials, Deakin University, Australia.
Low-JPEG Download (0.2MB)
High-JPEG Download (5.6MB)