Agilent Technologies' Automated DisplayPort Compliance Test Solution Supports ROHM's DisplayPort Rx LSI

  
  

The following product photos are available for use by the media, based on the Keysight Photography Use Policy.

The W2642A DisplayPort AUX channel controller enables fast and easy automated testing for the physical layer as well as flexible debug capability for new DisplayPort designs.

Image 1:
The W2642A DisplayPort AUX channel controller enables fast and easy automated testing for the physical layer as well as flexible debug capability for new DisplayPort designs.

Low-JPEG Download (0.1MB)

High-JPEG Download (0.6MB)

A key component in source or sink test solutions is the W2641A DisplayPort test point access adaptor

Image 2:
A key component in source or sink test solutions is the W2641A DisplayPort test point access adaptor.

Low-JPEG Download (0.1MB)

High-JPEG Download (0.3MB)

The Agilent DSO90000A Series oscilloscopes

Image 3:
The Agilent DSO90000A Series oscilloscopes

Low-JPEG Download (0.1MB)

High-JPEG Download (0.6MB)

The Agilent DisplayPort automation solution, seen here with the J-BERT N4903B, addresses the need for efficient and consistent certification processes in compliance test labs and enables fast design and margin analysis where repetitive measurements are required for temperature and design.

Image 4:
The Agilent DisplayPort automation solution, seen here with the J-BERT N4903B, addresses the need for efficient and consistent certification processes in compliance test labs and enables fast design and margin analysis where repetitive measurements are required for temperature and design.

Low-JPEG Download (0.3MB)

High-JPEG Download (4.1MB)

Agilent's precision BERT generators with independently controllable signal stress sources provide quality test results while enabling designers to efficiently control signal parameters.

Image 5:
Agilent's precision BERT generators with independently controllable signal stress sources provide quality test results while enabling designers to efficiently control signal parameters.

Low-JPEG Download (0.1MB)

High-JPEG Download (0.2MB)

This image is a screenshot of the DisplayPort compliance testing eye diagram and margin analysis. The distance from the center mask location is a measure of design margin and is reported as eye margin if the eye mask mode is chosen in the configuration screen.

Image 6:
This image is a screenshot of the DisplayPort compliance testing eye diagram and margin analysis. The distance from the center mask location is a measure of design margin and is reported as eye margin if the eye mask mode is chosen in the configuration screen.

Low-JPEG Download (0.1MB)

High-JPEG Download (0.3MB)

This image is a screenshot of the DisplayPort electrical test software results report, which documents your test, indicates the pass/fail status, the test specification range, the measured values, and the margin.

Image 7:
This image is a screenshot of the DisplayPort electrical test software results report, which documents your test, indicates the pass/fail status, the test specification range, the measured values, and the margin.

Low-JPEG Download (0.1MB)

High-JPEG Download (0.2MB)

Agilent N4915A DisplayPort ISI Generator

Image 8:
Agilent N4915A DisplayPort ISI Generator

Low-JPEG Download (0.1MB)

High-JPEG Download (0.2MB)

Agilent DisplayPort Sink Test Solution

Image 9:
Agilent DisplayPort Sink Test Solution

Low-JPEG Download (0.1MB)

High-JPEG Download (0.3MB)

 

Related Information
  Press Release:

Agilent Technologies' Automated DisplayPort Compliance Test Solution Supports ROHM's DisplayPort Rx LSI
(2010-February-23)

  Press Release:

Agilent Technologies and Quantum Data Solution Enables DisplayPort Test Automation
(2008-December-01)

  Press Release:

Agilent Technologies' DisplayPort Sink Test Platform Qualified by VESA
(2008-June-02)

  Press Release:

Agilent Technologies Demonstrates Industry's First Completely Automated DisplayPort Physical Layer Compliance Test Solution
(2008-April-08)

  Press Release:

Agilent Technologies Demonstrates Industry's First Completely Automated DisplayPort Physical Layer Compliance Test Solution
(2008-March-26)

  Press Release:

Agilent Technologies Expands its DisplayPort Test Capability
(2007-Decenber-5)

  Press Release:

Agilent Technologies Chosen by Allion Test Labs to Test Digital Display Technologies
(2007-December-5)

  Press Release:

Agilent Technologies Improves Industry's First DisplayPort Source Compliance, Characterization Test Solution
(2007-December-5)

  Keysight Photography Use Policy:

We will permit use of Keysight photography available via this site as long as the use will not disparage Keysight nor imply endorsement by Keysight. The photography cannot be changed or manipulated in any way with the exception of resizing or cropping. By downloading our product photography you are indicating that you accept these terms. Any commercial use of these images must be approved by Keysight Technologies.

ALL IMAGES USED MUST INDICATE:
"Reproduced with Permission, Courtesy of Keysight Technologies, Inc."

  How do I download images:

To download files in Windows, use the right mouse button on the desired format (JPEG or TIFF) and choose 'Save Target As...'