The following product photos are available for use by the media, based on the Keysight Photography Use Policy.
Image 1:
Accelerate 5G research with the new Keysight 5G Channel Sounding Reference Solution, a combination of hardware, software and programming examples.
Low-JPEG Download (0.7MB)
High-JPEG Download (1.0MB)
Image 2:
This image shows an AWG set up for the Tx in the Keysight Reference Solution IO control software.
Low-JPEG Download (0.4MB)
Image 3:
This image shows the Keysight Reference Solution instrument set up for the Rx in the IO control software.
Low-JPEG Download (0.3MB)
Image 4:
This image shows the Keysight Reference Solution IO control software for digitizer channel-to-channel corrections.
Low-JPEG Download (0.5MB)