Here’s the page we think you wanted. See search results instead:

 

Keysight Technologies 5G Channel Sounding, Reference Solution

  
  

The following product photos are available for use by the media, based on the Keysight Photography Use Policy.

Image 1:
Accelerate 5G research with the new Keysight 5G Channel Sounding Reference Solution, a combination of hardware, software and programming examples.

Low-JPEG Download (0.7MB)

High-JPEG Download (1.0MB)

Image 2:
This image shows an AWG set up for the Tx in the Keysight Reference Solution IO control software.

Low-JPEG Download (0.4MB)

Image 3:
This image shows the Keysight Reference Solution instrument set up for the Rx in the IO control software.

Low-JPEG Download (0.3MB)

Image 4:
This image shows the Keysight Reference Solution IO control software for digitizer channel-to-channel corrections.

Low-JPEG Download (0.5MB)

Related Information

Keysight Photography Use Policy:

We will permit use of Keysight photography available via this site as long as the use will not disparage Keysight nor imply endorsement by Keysight. The photography cannot be changed or manipulated in any way with the exception of resizing or cropping. By downloading our product photography you are indicating that you accept these terms. Any commercial use of these images must be approved by Keysight Technologies.

ALL IMAGES USED MUST INDICATE:
"Reproduced with Permission, Courtesy of Keysight Technologies, Inc."

How do I download images:

To download files in Windows, use the right mouse button on the desired format (JPEG or TIFF) and choose 'Save Target As...'