Agilent Technologies' New EXM Wireless Test Set Ready for Volume Production of LTE-Advanced, 802.11ac WLAN Devices

  
  

SANTA CLARA, Calif., Nov. 12, 2013

Agilent Technologies Inc. (NYSE: A) today announced the E6640A EXM wireless test set, which offers breakthrough manufacturing-test scalability in technology coverage, performance and capacity to test up to 32 cellular and wireless-connectivity devices in parallel. The EXM offers manufacturers the speed, accuracy and multi-port density to ramp up rapidly and optimize full-volume manufacturing. To accelerate test development, the EXM is synchronized with the latest cellular and WLAN chipsets.

"To solve today's manufacturing problems, our customers want the fastest, most accurate parallel device test to maximize throughput and yield," said Guy Séné, Agilent senior vice president and Electronic Measurement Group president. "The EXM addresses these needs, and as test requirements change, it offers modular scalability so manufacturers can evolve their test stations faster and keep pace with next-generation devices and standards at the lowest cost of test."

Offering the ultimate in scalability, the EXM can be configured with up to four independent transmit/receive (TRX) channels, each of which is a complete vector signal generator and vector signal analyzer. Each TRX includes four RF ports, two full-duplex and two half-duplex, to provide industry-leading port density. To further extend scalability and port density, the EXM can be customized to connect up to 32 devices-under-test through multi-port adapter (MPA) technology.

For today's highly integrated devices, the EXM offers 160-MHz bandwidth, up to 6-GHz frequency range, and the broadest choice of multi-format coverage, from LTE-Advanced in cellular to 802.11ac with multiple-input/multiple-output (MIMO) in wireless connectivity. The industry-proven Agilent X-Series measurement applications provide a wide range of standard-specific calibration and verification test capabilities.

To maximize production throughput, the EXM is equipped with a quad-core processor, high-bandwidth PXIe backplane and advanced sequence analyzer capabilities. To further reduce test time, the EXM includes the ability to make multiple measurements on a single set of acquired data.

Superior signal quality and excellent measurement accuracy ensure improvements in first-pass yield. For example, power-level accuracy is a best-in-class ±0.5 dB at 3.8 GHz, and the receiver EVM noise floor is -42 dB for 802.11ac.

The E6640A EXM is available to order now. Contact an Agilent sales representative for pricing information.

More information is available at www.agilent.com/find/EXM. High-resolution images are available at www.agilent.com/find/EXM_images. A short video describing the EXM and its capabilities is available at www.youtube.com/playlist?list=PLgv--LGySw06YeQ_kon19MYWCesfWQZDa.


About Agilent Technologies

Agilent Technologies Inc. (NYSE: A) is the world's premier measurement company and a technology leader in chemical analysis, life sciences, diagnostics, electronics and communications. The company's 20,500 employees serve customers in more than 100 countries. Agilent had revenues of $6.9 billion in fiscal 2012. Information about Agilent is available at www.agilent.com.

# # #

Contact:

Janet Smith, Americas
+1 970 679 5397
Twitter: @JSmithAgilent

Sarah Calnan, Europe
+44 (118) 927 5101
[email protected]

Iris Ng, Asia
+852 31977979
[email protected]