SANTA CLARA, Calif., July 1, 2014
Agilent Technologies Inc. (NYSE: A) today introduced the industry's first power device capacitance analyzer that automatically characterizes power device junction capacitances using real operating voltages.
With the increasing use of power devices fabricated from emerging materials like SiC and GaN, switching power supplies are now operating at increasingly higher frequencies. As a result, accurate device capacitance characterization is more important than ever. With its ability to accurately and automatically evaluate all input, output and reverse transfer power device capacitance at high bias voltages, Agilent's B1507A Power Device Capacitance Analyzer is well equipped to address this task.
The B1507A provides a complete solution for measuring and evaluating all parameters for high-frequency switching power supplies. Measurement capabilities include three terminal capacitances (Ciss, Coss and Crss) with high-voltage bias (+/-3 kV), gate resistance, and accurate leakage current and breakdown voltage by complementing curve-tracer-type test equipment that evaluates only coarse IV characteristics.
A uniquely designed intuitive graphical user interface makes it easy for even a novice user to automatically measure all capacitances under a wide range of operating voltages. Such capabilities make the B1507A ideal for helping power electronics circuit designers select the optimal devices for their power electronic circuits and for power electronics manufacturers maximizing product value and performance by revealing detailed device characteristics.
"Power devices used in power electronics circuits play a critical role in meeting industry requirements for low power loss and high switching frequency," said Masaki Yamamoto, general manager of Agilent's Hachioji Semiconductor Test Division. "However, until now no suitable solution has existed for fully evaluating their capacitance over a wide range of operating voltages. The B1507A promises to fill this gap by providing complete capacitance evaluation for power devices in a reliable and automated manner."
Some of the key features of the B1507A include:
U.S. Pricing and Availability
The Agilent B1507A Power Device Capacitance Analyzer is priced at $80,000 and available now.
More information is available at www.agilent.com/find/B1507A. A product image is available at www.agilent.com/find/B1507A_images.
Agilent Technologies Inc. (NYSE: A) is the world's premier measurement company and a technology leader in chemical analysis, life sciences, diagnostics, electronics and communications. The company's 20,600 employees serve customers in more than 100 countries. Agilent had revenues of $6.8 billion in fiscal 2013. Information about Agilent is available at www.agilent.com.
On Sept. 19, 2013, Agilent announced plans to separate into two publicly traded companies through a tax-free spinoff of its electronic measurement business. The new company is named Keysight Technologies, Inc. The separation is expected to be completed in early November 2014.
# # #
Contact:
Janet Smith, Americas
+1 970 679 5397
janet_smith@agilent.com
Twitter: @JSmithAgilent
Sarah Calnan, Europe
+44 (118) 927 5101
sarah_calnan@agilent.com
Connie Wong, Asia
+852 3197-7818
connie-ky_wong@agilent.com