SANTA CLARA, Calif., April 2, 2014
Agilent Technologies Inc. (NYSE: A) today expanded the world's most flexible PNA-X family of network analyzers with an 8.5 GHz model that more economically supports lower-frequency devices used in wireless communication applications (e.g., handsets, base stations, WLAN and other mobile communication devices).
Agilent's award-winning PNA-X nonlinear vector network analyzer (NVNA) has also been expanded to include an 8.5 GHz model. The new solutions provide engineers developing and manufacturing active devices the flexibility to select just the right frequency required for their specific application.
When characterizing active devices, the right mix of speed, performance and measurement integrity is critical to gaining a competitive edge. The new 8.5 GHz PNA-X offers both the unmatched performance and capabilities needed to deliver on all fronts. Moreover, its lower cost and frequency bring advanced measurement capabilities to the cost-sensitive wireless communication device market, where reduced test time, number of test stations and test cost are critical.
With low-noise amplifier tests there are typically multiple test stations, such as small signal gain/match, distortions and noise figure; the PNA-X integrates these test stations into one. By integrating measurements from multiple test stations into one, the PNA-X reduces the number of test stations by as much as 75 percent and reduces costs by 30 percent.
The new 8.5 GHz model also now brings the NVNA solution to engineers working in the RF and microwave frequency ranges. Agilent's NVNA is the industry's first measurement and simulation environment for designing nonlinear components. The result is the highest level of insight into nonlinear device behavior, making the NVNA capability especially useful for scientists researching new RF technologies and engineers involved in designing today's high-performance active devices. Using NVNA, X-parameters are measured and then used to create X-parameter models that can be imported into Agilent's Advanced Design System (ADS) to simulate actual linear and nonlinear component behavior.
"For today's wireless communication designers and manufacturers of RF components, finding a test system that meets their needs without forcing them to pay for functionality they don't want is paramount," said Steve Scheppelmann, Agilent's PNA marketing manager. "The new 8.5 GHz PNA-X model, coupled with the industry's widest range of measurement applications, now provides them the flexibility they need to build their optimal test solution."
Key features of the PNA-X Series network analyzers include:
U.S. Pricing and Availability
Agilent's new 8.5 GHz, 2- or 4-port PNA-X model and PNA-X NVNA option are now available. Pricing is as follows:
N5249A-200 | PNA-X network analyzer, |
$55,390 |
N5249A-219 | Extended power range and |
$6,135 |
N5249A-224 | Internal second source, combiner and |
$14,146 |
N5249A-400 | PNA-X network analyzer, |
$67,531 |
N5249A-419 | Extended power range and bias tees |
$11,332 |
N5249A-423 | Internal combiner and mechanical |
$6,221 |
The NVNA option prices start at $39,582.
More information about the new 8.5 GHz PNA-X model and breakthrough NVNA technology is available at www.agilent.com/find/pna and www.agilent.com/find/nvna, respectively. Photos of Agilent's expanded PNA-X solution are available at www.agilent.com/find/8.5GHz_PNA-X_images.
Agilent Technologies Inc. (NYSE: A) is the world's premier measurement company and a technology leader in chemical analysis, life sciences, diagnostics, electronics and communications. The company's 20,600 employees serve customers in more than 100 countries. Agilent had revenues of $6.8 billion in fiscal 2013. Information about Agilent is available at www.agilent.com.
On Sept. 19, 2013, Agilent announced plans to separate into two publicly traded companies through a tax-free spinoff of its electronic measurement business. The new company is named Keysight Technologies, Inc. The separation is expected to be completed in early November 2014.
# # #
Contact:
Janet Smith, Americas
+1 970 679 5397
janet_smith@agilent.com
Twitter: @JSmithAgilent
Sarah Calnan, Europe
+44 (118) 927 5101
sarah_calnan@agilent.com
Connie Wong, Asia
+852 3197-7818
connie-ky_wong@agilent.com