Agilent Technologies Announces New Handheld Thermal Imager and Insulation Resistance Testers for Predictive and Preventive Maintenance Applications

  
  

SANTA CLARA, Calif., June 2, 2014

Agilent Technologies Inc. (NYSE: A) today announced the addition of two new ranges of instruments to its portfolio of handheld tools. The U5855A TrueIR thermal imager provides clear and sharp thermal images with its unique Fine Resolution capability. The U1450A/60A Series offers five models of insulation resistance testers with wireless testing and report generation capability.



With the shift toward predictive maintenance, the U5855A TrueIR thermal imager allows engineers to safely and efficiently identify potential faults without shutting down the systems or disrupting the productivity of an industrial plant. The U5855A comes with Fine Resolution capability, which enhances the quality of thermal images by reconstructing the image based on multiple continuously captured infrared frames. This allows the U5855A to achieve an effective image resolution of 320 x 240 pixels from a 160 x 120 pixel detector. With this feature, the U5855A provides four times more resolution than typical 160 x 120 thermal imagers. Together with a 4x digital zoom, the U5855A reveals finer details, especially when inspecting small cracks on industrial pipelines even from a distance away.

The U5855A's light and ergonomic design allows engineers to comfortably use the thermal imager for longer periods of time, and operate it single-handedly in tight locations. Users can also easily change settings or access frequently used functions such as torch light and laser pointer, auto scaling or trigger with quick access buttons. With in-camera monitoring and analysis capabilities, the U5855A saves time by eliminating the need to connect to a PC. For more in-depth analysis and report generation, engineers can use the TrueIR Analysis and Reporting Tool PC software, which can be downloaded free of charge by visiting www.agilent.com/find/TrueIR_ART.

The U1450A/60A Series are 1 kV insulation resistance testers that measure leakage current and insulation resistance for preventive maintenance applications, such as checking the integrity of windings or cables in motors, transformers and electrical installations. The U1450A/60A Series comes with report-generation software that engineers can use to produce error-free automated test reports in table and graph forms. All five models are certified to IP 67 and are compatible with the Agilent remote link solution, enabling wireless remote insulation testing.

For applications that require unique test voltages, the U1450A/60A Series offers two models with adjustable test voltage ranges from 10 V to 1.1 kV, with 1 V step increments. A two-in-one insulation tester model with a 4.5 digit full-featured digital multimeter is also available.

"We have come a long way since the launch of our first handheld product in 2006, and with the U5855A TrueIR thermal imager, we have expanded our reach into predictive maintenance for industrial applications and building maintenance," said Ee Huei Sin, vice president, Agilent's General-Purpose Electronic Measurement Division. "With these two new handheld solutions, we continue to fulfill our ongoing commitment of creating more dependable tools with essential capabilities."

About Agilent Remote Link Solution

The remote link solution is Agilent's next generation wireless connectivity solution. By simply attaching the U1177A or U1117A infrared-to-Bluetooth(r) adapter to a compatible Agilent handheld meter, engineers are able to remotely measure, view and test measurements from the new U1115A remote logging display, iOS/Android smart devices or on a Windows PC. The new U1117A also comes with an extended range of up to 100 meters (300 feet), enabling safer and more convenient testing in hazardous environments.

More information is available at www.agilent.com/find/hhgowireless_pr.

U.S. Pricing and Additional Information

The new U5855A TrueIR thermal imager and U1450A/60A Series handheld insulation resistance testers are available worldwide, at the prices listed below:

Product

Model

Description

Price

Thermal imager

U5855A

TrueIR thermal imager

$3,500

Insulation resistance tester

U1451A

Insulation resistance tester, 250 V to 1 kV

$500

U1452A

Insulation resistance tester, 50 V to 1 kV

$697

U1452AT

Telecommunications insulation resistance tester, 50 V to 100 V

$597

U1453A

Insulation resistance tester, OLED display, 50 V to 1 kV

$790

U1461A

Insulation multimeter, OLED display, 50 V to 1 kV

$890

 

Information on the U5855A TrueIR thermal imager is available at www.agilent.com/find/trueIRimager_pr. High-resolution images are available at www.agilent.com/find/trueIRimager_images.

Find out more about the U1450A/60A Series handheld insulation resistance testers at www.agilent.com/find/insulationtesters_pr. High-resolution images available at www.agilent.com/find/insulationtesters_images.


About Agilent Technologies

Agilent Technologies Inc. (NYSE: A) is the world's premier measurement company and a technology leader in chemical analysis, life sciences, diagnostics, electronics and communications. The company's 20,600 employees serve customers in more than 100 countries. Agilent had revenues of $6.8 billion in fiscal 2013. Information about Agilent is available at www.agilent.com.

On Sept. 19, 2013, Agilent announced plans to separate into two publicly traded companies through a tax-free spinoff of its electronic measurement business. The new company is named Keysight Technologies, Inc. The separation is expected to be completed in early November 2014.

# # #

Contact:

Janet Smith, Americas
+1 970 679 5397
[email protected]
Twitter: @JSmithAgilent

Sarah Calnan, Europe
+44 (118) 927 5101
[email protected]

Connie Wong, Asia
+852 3197-7818
[email protected]