SANTA CLARA, Calif., June 2, 2014
Agilent Technologies Inc. (NYSE: A) today announced that the Agilent EEsof EDA W1918 LTE-Advanced baseband verification library has added support for key 4G technologies, such as Adaptive Modulation and Coding (AMC) and Coordinated Multi-Point (CoMP).
The new modeling and simulation capability enables wireless system architects to model sophisticated dynamic behaviors and realistic performance at cell edges according to the physical layer (PHY) specifications of 3GPP Releases 10 and 11. This accelerates the design and verification process for 4G chipsets and infrastructure, enabling faster deployment.
The newly supported 4G technologies enable wireless infrastructure to tailor signals in marginal coverage areas to a particular mobile phone, using adaptive and cooperative techniques that go beyond simple 1:1 interaction between the transmitter and receiver. This dynamic behavior makes validation of the PHY algorithms, RF components and link-level throughput progressively more difficult in R&D-both in EDA simulations as well as test equipment-because negotiation and interaction are often required. That is, a complete working system is required to verify baseband algorithms, RF components and throughput under realistic conditions, making this process problematic in early R&D, prior to final hardware integration and test.
The SystemVue simulation environment, Agilent's premier platform for electronic system-level design, is able to reproduce these conditions in R&D with the help of the W1918 LTE-Advanced library. Updates to the W1918 library include:
"SystemVue stands alone as a development platform that can pull together sophisticated 'executable' standards references like LTE-Advanced Release 11, accurate RF models, wideband test equipment links, and open algorithm modeling interfaces such as MATLAB, C++ and HDL," said Frank Ditore, SystemVue product planner at Agilent. "As the industry moves toward 5G, all of these modeling domains are getting more difficult. Agilent is pleased to offer a platform that is truly ready today for 5G innovation."
SystemVue and its updated W1918 LTE-Advanced library will be shown at IMS 2014/IEEE MTT-S (Booth 1133), June 1-6 in Tampa, Florida, and at DAC 2014 (Booth 419), June 2-4 in San Francisco.
U.S. Pricing and Availability
Agilent's W1918 LTE-Advanced baseband verification library, part of SystemVue 2013.08 Service Pack 1, is available for download at www.agilent.com/find/eesof-systemvue-latest-downloads. This update to the W1918 library is expected in early June. Pricing for the SystemVue environment starts at approximately $17,687. A free, 30-day evaluation copy of SystemVue is available at www.agilent.com/find/eesof-systemvue-evaluation. An image of SystemVue 2013.08 SP1 with its LTE-Advance library is available at www.agilent.com/find/SystemVueLTEA_images.
About Agilent EEsof EDA Software
Agilent EEsof EDA is the leading supplier of electronic design automation software for microwave, RF, high-frequency, high-speed digital, RF system, electronic system level, circuit, 3-D electromagnetic, physical design and device-modeling applications. More information is available at www.agilent.com/find/eesof.
Agilent Technologies Inc. (NYSE: A) is the world's premier measurement company and a technology leader in chemical analysis, life sciences, diagnostics, electronics and communications. The company's 20,600 employees serve customers in more than 100 countries. Agilent had revenues of $6.8 billion in fiscal 2013. Information about Agilent is available at www.agilent.com.
On Sept. 19, 2013, Agilent announced plans to separate into two publicly traded companies through a tax-free spinoff of its electronic measurement business. The new company is named Keysight Technologies, Inc. The separation is expected to be completed in early November 2014.
# # #
Contact:
Janet Smith, Americas
+1 970 679 5397
[email protected]
Twitter: @JSmithAgilent
Sarah Calnan, Europe
+44 (118) 927 5101
[email protected]
Connie Wong, Asia
+852 3197-7818
[email protected]