SANTA CLARA, Calif., Feb. 3, 2014
Agilent Technologies Inc. (NYSE: A) today introduced the E5063A PCB Analyzer for printed circuit board impedance test in manufacturing. The solution offers technology breakthroughs in accuracy and repeatability and reproducibility (R&R). The analyzer also provides a dedicated user interface with broader language support, and more robustness against electrostatic discharge for PCB manufacturing environments.
Tighter impedance tolerance is a direct result of increasing data rates; more accurate impedance test solutions for PCB manufacturing is now required to achieve signal integrity. The E5063A PCB Analyzer meets that demand by providing advanced error-correction methods to enhance measurement accuracy and R&R. These enhancements help improve yield for PCB impedance test.
Option 011 in the E5063A PCB Analyzer now supports simplified and traditional Chinese, Japanese and Korean, providing easier access and operation in global installations.
The ESD protection circuit now available on the E5063A PCB Analyzer helps overcome the serious ESD damage that traditional PCB measurement solutions can encounter. The highly robust architecture of E5063A protects the instrument from ESD damage, minimizing downtime and repair.
"In addition to enhancements that go beyond traditional test solutions, we offer the solution at an affordable price," said Akira Nukiyama, vice president and general manager, Agilent's Component Test Division. "Continuous achievements in high-speed digital applications and uncompromising expertise in RF measurements enable us to achieve these breakthroughs with the E5063A PCB Analyzer."
U.S. Pricing and Additional Information
E5063A-011 Time domain analysis/Test wizard option: $10,000
E5063A PCB Analyzer frequency options:
E5063A-245 | 2-port test set, 100 kHz to 4.5 GHz | $18,600 |
E5063A-285 | 2-port test set, 100 kHz to 8.5 GHz | $26,800 |
E5063A-2H5 | 2-port test set, 100 kHz to 18 GHz | $35,100 |
Information on the E5063A PCB Analyzer can be found at www.agilent.com/find/ena-pcb. High-resolution images are available at www.agilent.com/find/E5063APCB_images.
Agilent Technologies Inc. (NYSE: A) is the world's premier measurement company and a technology leader in chemical analysis, life sciences, diagnostics, electronics and communications. The company's 20,600 employees serve customers in more than 100 countries. Agilent had revenues of $6.8 billion in fiscal 2013. Information about Agilent is available at www.agilent.com.
On Sept. 19, 2013, Agilent announced plans to separate into two publicly traded companies through a tax-free spinoff of its electronic measurement business. The new company is named Keysight Technologies, Inc. The separation is expected to be completed in early November 2014.
# # #
Contact:
Janet Smith, Americas
+1 970 679 5397
[email protected]
Twitter: @JSmithAgilent
Sarah Calnan, Europe
+44 (118) 927 5101
[email protected]
Iris Ng, Asia
+852 31977979
[email protected]