SANTA CLARA, Calif., Feb. 3, 2014
Agilent Technologies Inc. (NYSE: A) today announced the E5063A ENA Series network analyzer, a low-cost ENA solution for manufacturing test. The instrument offers optimized performance and functionality for testing simple RF passive components, such as handset/BTS antennas, RF cables and filters. It can also be used in R&D for evaluation of RF passive devices and dielectric materials.
The Agilent E5063A offers the best balance of performance and cost. It provides excellent RF performance, including trace noise of 0.002 dBrms and the stability of 0.01 dB/degC. This feature helps reduce test cost without sacrificing quality.
Using the E5063A with U1810B USB RF switch, engineers can build an economical multi-DUT test solution for testing four antennas with a single instrument, further reducing cost of test.
With proven calibration and data analysis capabilities, including the fixture simulator function, the E5063A provides measurements consistent with the industry-standard Agilent E5071C ENA Series network analyzer.
The combination of the E5063A and the 85070E dielectric probe kit offers an ideal economical solution for characterizing dielectric material, making it suitable for material researchers with limited budgets.
"The new Agilent E5063A ENA Series network analyzer addresses the need to drive down the total cost of test for both the manufacturing and R&D environments," said Akira Nukiyama, vice president and general manager, Agilent's Component Test Division. "It is an optimized solution without compromising performance or quality."
U.S. Pricing and Additional Information
The Agilent E5063A ENA Series network analyzer pricing options include:
E5063A-245 | 2-port test set, 100 kHz to 4.5 GHz | $18,600 |
E5063A-285 | 2-port test set, 100 kHz to 8.5 GHz | $26,800 |
E5063A-2H5 | 2-port test set, 100 kHz to 18 GHz | $35,100 |
Information on the E5063A ENA Series network analyzer can be found at www.agilent.com/find/e5063a. High-resolution images are available at www.agilent.com/find/E5063A_images.
A trade-up program is available for legacy vector network analyzers, including the Agilent 8753. The new E5063A provides better dynamic range and trace noise performance at a lower cost than the previous industry-standard RF network analyzer.
Agilent Technologies Inc. (NYSE: A) is the world's premier measurement company and a technology leader in chemical analysis, life sciences, diagnostics, electronics and communications. The company's 20,600 employees serve customers in more than 100 countries. Agilent had revenues of $6.8 billion in fiscal 2013. Information about Agilent is available at www.agilent.com.
On Sept. 19, 2013, Agilent announced plans to separate into two publicly traded companies through a tax-free spinoff of its electronic measurement business. The new company is named Keysight Technologies, Inc. The separation is expected to be completed in early November 2014.
# # #
Contact:
Janet Smith, Americas
+1 970 679 5397
janet_smith@agilent.com
Twitter: @JSmithAgilent
Sarah Calnan, Europe
+44 (118) 927 5101
sarah_calnan@agilent.com
Iris Ng, Asia
+852 31977979
iris-hw_ng@agilent.com