SANTA CLARA Calif., and BEAVERTON, Ore., June 3, 2014
Agilent Technologies Inc. (NYSE: A) and Cascade Microtech, Inc. (NASDAQ: CSCD) today announced a strategic alliance to provide fully configured and validated RF measurement solutions that streamline wafer-level semiconductor measurements while delivering guaranteed configuration, installation and support.
"Agilent and Cascade Microtech are the worldwide leaders in test and measurement and on-wafer probing, offering both the expertise and products to provide all the building blocks for wafer-level device testing," said Gregg Peters, vice president and general manager of Agilent's Component Test Division. "By aligning our efforts and respective solutions, we are pioneering a new model for the delivery of uniquely differentiated wafer-level measurement solutions to our mutual semiconductor customers."
From Configuration to Accurate, Validated Measurements
Specifying and configuring a wafer-level RF measurement system can be challenging and time-consuming, often requiring equipment to be sourced from multiple suppliers and then configured and verified on-site by the customer. As a result, the time to first measurement can be long. With wafer-level measurement solutions (WMS) from Agilent and Cascade Microtech, semiconductor customers now have the equipment they need to perform accurate and repeatable DC and RF measurements, device characterization and modeling, all while realizing significant time savings to first measurement.
"Semiconductor process development, modeling and characterization tasks are evolving, time-to-market cycles are shrinking, and the need for greater accuracy is increasing," said Michael Burger, president and chief executive officer of Cascade Microtech. "By working with Agilent to provide guaranteed wafer-level measurement solutions, we can now provide semiconductor engineers the tools they need to perform accurate and fast advanced DC and RF measurements on both components and devices to get their products to market on time."
The new wafer-level measurement solutions combine Cascade Microtech's wafer probe stations, probes and calibration tools with Agilent's test instrumentation and measurement and analysis software. Each solution configuration is pre-validated to ensure it meets customers' specific application needs, then validated again-based on previously agreed-upon acceptance criteria-after installation by Cascade Microtech solutions experts. Guaranteed configuration means that any parts missing from the configured solution will be provided by either Agilent or Cascade Microtech, free of charge.
Agilent and Cascade Microtech have also collaborated to deliver unique workflow solutions software based on Agilent's WaferPro-XP measurement software. Together with Cascade Microtech's Velox probe station software, customers can now develop complete wafer test suites for a variety of measurement needs (e.g., S-parameters, DC-IV/CV, noise figure, Flicker noise, and gain compression). This combination of software provides a coherent environment for test development.
Each wafer-level measurement solution is backed by the offer of a full support package, with access to regional solution experts who are highly skilled in on-wafer test and measurement. Cascade Microtech acts as the single point of contact to ensure quick problem resolution.
Pricing and Availability
Agilent and Cascade Microtech wafer-level RF measurement solutions are now available in a range of configurations, from a fully integrated new solution with either a semi-automated or manual prober, to application-specific hardware upgrades to existing probe stations. Agilent's new WaferPro-XP measurement software platform for R&D device characterization can also be added to an existing wafer-level measurement solution. Pricing depends on solution configuration. For specific pricing and sales information, contact your local Agilent field engineer or Cascade Microtech sales manager.
More information on the new Agilent and Cascade Microtech wafer-level measurement solutions is available at www.agilent.com/find/wms and www.cascademicrotech.com/measureone. Photos are available at www.agilent.com/find/wms_images. A backgrounder is available at www.agilent.com/find/wms_backgrounder.
About Cascade Microtech, Inc.
Cascade Microtech, Inc. (NASDAQ: CSCD) is a worldwide leader in precision contact, electrical measurement and test of integrated circuits (ICs), optical devices and other small structures. For technology businesses and scientific institutions that need to evaluate small structures, Cascade Microtech delivers access to electrical data from wafers, ICs, IC packages, circuit boards and modules, MEMS, 3D TSV, LED devices and more. Cascade Microtech's leading-edge stations, probes, probe cards, advanced thermal subsystems and integrated systems deliver precision accuracy and superior performance both in the lab and during production manufacturing of high-speed and high-density semiconductor chips. For more information visit www.cascademicrotech.com.
Agilent Technologies Inc. (NYSE: A) is the world's premier measurement company and a technology leader in chemical analysis, life sciences, diagnostics, electronics and communications. The company's 20,600 employees serve customers in more than 100 countries. Agilent had revenues of $6.8 billion in fiscal 2013. Information about Agilent is available at www.agilent.com.
On Sept. 19, 2013, Agilent announced plans to separate into two publicly traded companies through a tax-free spinoff of its electronic measurement business. The new company is named Keysight Technologies, Inc. The separation is expected to be completed in early November 2014.
# # #
Contact:
Janet Smith, Americas
+1 970 679 5397
janet_smith@agilent.com
Twitter: @JSmithAgilent
Sarah Calnan, Europe
+44 (118) 927 5101
sarah_calnan@agilent.com
Connie Wong, Asia
+852 3197-7818
connie-ky_wong@agilent.com
Debbora Ahlgren, Cascade Microtech
+1 503 601 1000
Debbora.Ahlgren@cmicro.com