SANTA CLARA, Calif., June 4, 2014
Agilent Technologies Inc. (NYSE: A) today announced enhancements to the N9000A CXA X-Series signal analyzer that broaden its use in RF and microwave applications. The CXA platform now supports the Windows 7 operating system, giving it better performance and stability.
Additional enhancements include RF CXA phase noise that now provides up to a 10 dB performance improvement, enhancing test result accuracy. For microwave frequencies, the CXA supports new cellular telecommunications, wireless connectivity and digital video measurement applications. Also, there is now an extension to the analyzer's operating temperature range for guaranteed performance between 0°C to 55°C.
"The CXA entered the market as a high-quality, low-cost solution," said Brian LeMay, general manager of Agilent's Chengdu Instruments Division. "The latest enhancements add to its capabilities and value, delivering an affordable signal analyzer with even more features typically associated with higher-cost products."
Enhancements for the RF CXA analyzer:
Enhancements for the microwave CXA analyzer include:
U.S. Pricing and Availability
The Agilent N9000A signal analyzer starts at $13,259 and varies based on a customer's specific test system requirements; contact Agilent at (800) 829-4444 for more information. All new orders beginning June 1 will include Windows 7 as standard (W7X). Detailed product information is available at www.agilent.com/find/cxa. High-resolution images are available at www.agilent.com/find/cxa3.5_images.
Agilent Technologies Inc. (NYSE: A) is the world's premier measurement company and a technology leader in chemical analysis, life sciences, diagnostics, electronics and communications. The company's 20,600 employees serve customers in more than 100 countries. Agilent had revenues of $6.8 billion in fiscal 2013. Information about Agilent is available at www.agilent.com.
On Sept. 19, 2013, Agilent announced plans to separate into two publicly traded companies through a tax-free spinoff of its electronic measurement business. The new company is named Keysight Technologies, Inc. The separation is expected to be completed in early November 2014.
# # #
Contact:
Janet Smith, Americas
+1 970 679 5397
[email protected]
Twitter: @JSmithAgilent
Sarah Calnan, Europe
+44 (118) 927 5101
[email protected]
Connie Wong, Asia
+852 3197-7818
[email protected]