SANTA CLARA, Calif., March 4, 2014
Agilent Technologies Inc. (NYSE: A) today introduced a high-performance 14-slot AXIe chassis and system module. This unique technology enables multi-module system capabilities that allow test engineers working in radar, antenna, high-energy physics and digital to set up large systems with all modules in a single chassis, providing better module-to-module synchronization and performance.
Agilent's new M9514A AXIe chassis and M9521A system module provide a high-performance platform for large channel count systems with a single connection to the host computer. A test engineer can connect multiple AXIe and PXIe chassis for ultimate system-design flexibility.
"We are the first to deliver a high-performance AXIe chassis enabling large systems and phase-coherent measurements across many modules," said Agilent's Mario Narduzzi, marketing manager, Software and Module Solutions Division. "Our goal is to develop and deliver innovative modular solutions that enable customers to meet their unique development requirements."
The 14-slot M9514A AXIe chassis and M9521A system module meet AXIe 1.0 and 2.0 specifications and provide:
Instrument control is enabled through a soft front panel and programmatic interfaces tuned to the user's choice of application development environment. Using Agilent's IO Libraries Suite allows fast and easy integration into existing test environments.
Agilent's rapid repair turnaround-with industry-leading calibration core exchange strategy and standard three-year warranty-maximizes system uptime to reduce the total cost of ownership.
The M9514A AXIe 14-slot chassis and M9521A AXIe system module are the latest additions to Agilent's growing lineup of more than 60 PXI and AXIe modular products.
U.S. Pricing and Availability
The Agilent M9514A AXIe 14-slot chassis is $38,000, and the Agilent M9521A AXIe System Module is $8,000. Both products are available now.
Additional information about Agilent’s modular test solutions is available at www.agilent.com/find/M9514A and www.agilent.com/find/M9521A.
Product photos are available at www.agilent.com/find/M9514A_images and www.agilent.com/find/M9521A_images.
Agilent offers a complete lineup of PXI and AXIe products, including digitizers, arbitrary waveform generators, digitizing oscilloscopes, digital multimeters and a range of switches.
Agilent Technologies Inc. (NYSE: A) is the world's premier measurement company and a technology leader in chemical analysis, life sciences, diagnostics, electronics and communications. The company's 20,600 employees serve customers in more than 100 countries. Agilent had revenues of $6.8 billion in fiscal 2013. Information about Agilent is available at www.agilent.com.
On Sept. 19, 2013, Agilent announced plans to separate into two publicly traded companies through a tax-free spinoff of its electronic measurement business. The new company is named Keysight Technologies, Inc. The separation is expected to be completed in early November 2014.
# # #
Contact:
Janet Smith, Americas
+1 970 679 5397
[email protected]
Twitter: @JSmithAgilent
Sarah Calnan, Europe
+44 (118) 927 5101
[email protected]
Connie Wong, Asia
+852 3197 7818
[email protected]