SANTA CLARA, Calif., March 4, 2014
Agilent Technologies Inc. (NYSE: A) today introduced the M9037A, the fastest, highest-performance PXIe controller available. The controller's 12 GB/s maximum data bandwidth offers unique capability for complex or multi-chassis systems and secure environments. With best-in-class CPU processing speed and a front-panel removable 240 GB solid-state drive, it provides the performance, reliability and security required for aerospace/defense, RF, semiconductor, wireless communications, general-purpose, electronic functional test, or virtually any PXIe modular test system application.
The M9037A controller's 12 GB/s data bandwidth from the CPU to the PXIe backplane switch is achieved using the PCIe with a potential of up to 24 PCIe lanes. Based on Intel's i7-4700EQ extended life processor, the M9037A provides the fastest CPU computational measurements available. It offers a front panel x8 PCIe high-bandwidth connection to external PCIe devices, such as a second PXIe chassis or a RAID storage device, providing a unique alternative to using a valuable PXIe instrument slot.
"Our next-generation controller demonstrates Agilent's ongoing commitment to develop powerful, new products, adding features to our modular platform," said Agilent's Mark Pierpoint, vice president and general manager of the Software and Modular Solutions division. "By incorporating the fastest processor available, we are accelerating our customers' application capabilities and allowing them to easily connect to multiple chassis, external storage devices, and other modular and LXI instruments. This results in improvements in throughput and cost savings."
U.S. Pricing and Availability
The Agilent M9037A PXIe controller is available now. The base price is $6,950.
More information is available at www.agilent.com/find/m9037a. High-resolution images are available at www.agilent.com/find/m9037a_images.
Agilent Technologies Inc. (NYSE: A) is the world's premier measurement company and a technology leader in chemical analysis, life sciences, diagnostics, electronics and communications. The company's 20,600 employees serve customers in more than 100 countries. Agilent had revenues of $6.8 billion in fiscal 2013. Information about Agilent is available at www.agilent.com.
On Sept. 19, 2013, Agilent announced plans to separate into two publicly traded companies through a tax-free spinoff of its electronic measurement business. The new company is named Keysight Technologies, Inc. The separation is expected to be completed in early November 2014.
# # #
Contact:
Janet Smith, Americas
+1 970 679 5397
[email protected]
Twitter: @JSmithAgilent
Sarah Calnan, Europe
+44 (118) 927 5101
[email protected]
Connie Wong, Asia
+852 3197-7818
[email protected]