SANTA ROSA, Calif., Nov. 4, 2014
Keysight Technologies, Inc. (NYSE: KEYS) today introduced 200-, 300- and 500-MHz, high-voltage probing solutions with a wider input range, higher common-mode rejection ratio and optimized accessories. The probes are ideal for testing today's switching power supplies or power devices and for measuring motor drives and vehicle buses.
The Keysight N2804A differential probe offers up to 300-MHz bandwidth and ±300-Vdc + peak AC of the maximum differential input range, allowing engineers to use it for a broad range of power applications. The N2805A 200-MHz differential probe comes with a 5-m input cable, which allows engineers to easily reach DUTs over long distances.
The probes have a differential input resistance of 4 MΩ and low input capacitance of 4 pF to minimize circuit loading. The N2804A and N2805A probes are compatible with Keysight oscilloscopes with a 50-Ω AutoProbe interface, which automatically configures the scope for the probe.
The Keysight 10076C 100:1 passive probe with 66.7-MΩ input resistance provides the voltage and bandwidth engineers need for making high-voltage measurements referenced to the ground with low input loading. The probe provides 500-MHz bandwidth when used in conjunction with a spring ground tip to reduce inductive ground loading.
Information about the Keysight N2804A and N2805A differential probes is available at www.keysight.com/find/differential. Information about the Keysight 10076C passive probe is available at www.keysight.com/find/10076C. Photographs of the N2804A, N2805A and 10076C probes are available at www.keysight.com/find/highvoltageprobing_images .
U.S. Pricing and Availability
The Keysight N2804A and N2805A differential probes are available now at a price of $2,300 and $2,500 respectively. The 10076C passive probe is available now and is priced at $450.On Sept. 19, 2013, Agilent Technologies announced plans to separate into two publicly traded companies through a tax-free spinoff of its electronic measurement business. The new company, Keysight Technologies, began operating as a wholly owned subsidiary of Agilent on Aug. 1, 2014 with a full separation anticipated in early November 2014. Keysight is expected to trade on the NYSE under the symbol KEYS.
Keysight is a global electronic measurement technology and market leader helping to transform its customers' measurement experience through innovation in wireless, modular, and software solutions. Keysight provides electronic measurement instruments and systems and related software, software design tools and services used in the design, development, manufacture, installation, deployment and operation of electronic equipment. Information about Keysight is available at www.keysight.com.
# # #
Contact:
Janet Smith, Americas
+1 970 679 5397
[email protected]
Twitter: @KeysightJSmith
Sarah Calnan, Europe
+44 (118) 927 5101
[email protected]
Connie Wong, Asia
+852 3197-7818
[email protected]