SANTA CLARA, Calif., March 5, 2014
Agilent Technologies Inc. (NYSE: A) today announced that its 89600 VSA software has been enhanced with custom IQ modulation analysis. The analysis capability speeds time to insight by allowing R&D engineers to more easily test proprietary signals for satellite and military communication applications.
Due to security concerns, engineers developing SATCOM and MILCOM applications typically use proprietary and non-standardized signals. Testing these signals using a general-purpose tool can be very time-consuming. Engineers often have to develop their own algorithms, which must then be modified for each domain (e.g., analog, digital and RF) and different hardware drivers.
Agilent's new custom IQ modulation analysis simplifies this process by allowing engineers to create custom signal mapping that can be used to verify transmitters and also serves as a reference receiver for proprietary signals, enabling more accurate measurements. In addition, because the VSA software works across multiple platforms, there is no need rewrite code to accommodate different formats and drivers, further streamlining signal measurements.
"As a demonstrated leader in vector signal analysis, Agilent consistently innovates the 89600 VSA software to meet customers' needs," said Jim Curran, marketing manager of Agilent's Microwave and Communications Division. "With the addition of custom IQ modulation analysis, we're addressing the complex proprietary signal requirements of R&D engineers who design and troubleshoot applications in the A/D and satellite industries."
Agilent's 89600 VSA software is a comprehensive set of tools for signal demodulation and vector signal analysis that provide simultaneous views of virtually every facet of complex signals. This critical information enables engineers to achieve the clarity needed to find the root cause of signal problems. The software runs on a PC or inside PC-based instruments. It works with spectrum analyzers, signal analyzers, oscilloscopes, logic analyzers and modular instrument systems, as well as simulation software.
U.S. Pricing and Availability
The new custom IQ modulation analysis option (BHK) for the 89600 VSA software is now available for $4,000. A 45-day free trial of a fully featured version of the 89600 VSA, with no functionality restrictions, can be downloaded from the Trials and Licenses tab on at www.agilent.com/find/89600.
More information on the software and its new analysis capability is available at www.agilent.com/find/vsa_enhancements. An image of the analysis capability is available at www.agilent.com/find/89600vsa_images.
Agilent Technologies Inc. (NYSE: A) is the world's premier measurement company and a technology leader in chemical analysis, life sciences, diagnostics, electronics and communications. The company's 20,600 employees serve customers in more than 100 countries. Agilent had revenues of $6.8 billion in fiscal 2013. Information about Agilent is available at www.agilent.com.
On Sept. 19, 2013, Agilent announced plans to separate into two publicly traded companies through a tax-free spinoff of its electronic measurement business. The new company is named Keysight Technologies, Inc. The separation is expected to be completed in early November 2014.
# # #
Contact:
Janet Smith, Americas
+1 970 679 5397
janet_smith@agilent.com
Twitter: @JSmithAgilent
Sarah Calnan, Europe
+44 (118) 927 5101
sarah_calnan@agilent.com
Connie Wong, Asia
+852 3197-7818
connie-ky_wong@agilent.com