SANTA CLARA, Calif., May 5, 2014
Agilent Technologies Inc. (NYSE: A) today announced an enhancement to the Agilent 14585A control and analysis software for advanced power supplies, adding support for the N7900 Advanced Power System (APS) dynamic DC power supplies.
The N7900 Series power supplies with VersaPower architecture offer industry-leading features and specifications for fast operation, advanced measurements, and integrated features to reduce development time and support costs. These 1- and 2-kW models, expandable to 10 kW, were designed for applications where high-speed dynamic sourcing and measurement is needed.
The Agilent 14585A software enhances the user experience of the APS N7900 Series, giving R&D engineers access to the power supplies' advanced functionality without having to write a single line of code. The engineers can now perform complex tasks, such as waveform creation or long-term data logging, in a matter of minutes, with just a few clicks.
The 14585A Control & Analysis Software for Advanced Power Supplies supports the
N6705B DC Power Analyzer and now the APS N7900 Series dynamic DC power supplies.
"We are excited to meet the needs of our customers who require high power in R&D," said Kari Fauber, general manager of Agilent's Power and Energy Division. "Now that the 14585A software supports our Advance Power System N7900 Series, R&D engineers working on high-power devices no longer need to spend time being programmers."
The advanced functionality of the 14585A software includes:
The industry-leading specifications and advanced measurement capabilities of the APS N7900 Series include:
Additional information
U.S. Pricing and Availability
The N7900 APS dynamic DC power supplies are available now. Prices start at $9,900.
The Agilent 14585A Control & Analysis Software for Advanced Power Supplies is available now. A free 30-day trial is built into the software. After the free trial, a license is $1,267.
Agilent Technologies Inc. (NYSE: A) is the world's premier measurement company and a technology leader in chemical analysis, life sciences, diagnostics, electronics and communications. The company's 20,600 employees serve customers in more than 100 countries. Agilent had revenues of $6.8 billion in fiscal 2013. Information about Agilent is available at www.agilent.com.
On Sept. 19, 2013, Agilent announced plans to separate into two publicly traded companies through a tax-free spinoff of its electronic measurement business. The new company is named Keysight Technologies, Inc. The separation is expected to be completed in early November 2014.
# # #
Contact:
Janet Smith, Americas
+1 970 679 5397
[email protected]
Twitter: @JSmithAgilent
Sarah Calnan, Europe
+44 (118) 927 5101
[email protected]
Connie Wong, Asia
+852 3197-7818
[email protected]