SANTA ROSA, Calif., Oct. 7, 2014
Keysight Technologies, Inc. today announced the U2040 X-Series wide dynamic range power sensors, consisting of four USB models for wireless and radar applications, and a dedicated LAN model for satellite testing. With the world's widest dynamic range found in a power sensor and extremely high measurement speed, the U2040 X-Series makes fast, accurate and repeatable power measurements over a wide range of power levels, allowing engineers to improve productivity and lower cost of test.
The U2040 X-Series' 96 dB dynamic range, spanning -70 dBm to +26 dBm, enables accurate power measurements of very small signals, critical for applications such as wireless chipset and power amplifier module manufacturing. With the new average mode time selectivity feature, users are able to make both average and time selectivity average power measurements across the full 96 dB dynamic range. This is a significant improvement when compared to conventional power sensors, which often limit time-gated dynamic range measurements at around 50 dB.
With a measurement speed of up to 10,000 readings per second in fast/buffer mode, the U2040 X-Series measures continuously in real time and keeps pace with very fast pulses, up to 10 kHz pulse repetition frequency (PRF). While conventional sensors only provide a snapshot of continuous pulses, leaving dead time where glitches can slip by unnoticed, U2040 X-Series sensors measure every continuous pulse without leaving time gaps in between measurement acquisitions.
The U2040 X-Series provides broadband coverage for any modulated signal, and covers all common wireless signal formats such as LTE, LTE-Advanced with 100 MHz bandwidth, and WLAN 802.11ac with 80/160 MHz bandwidth. Built-in radar and wireless presets allow faster test set up, and for data capture and analysis, engineers can use the Keysight BenchVue software, which is bundled free of charge with each sensor.
"The U2040 X-Series achieves the world's widest dynamic range and enables seamless range transition with high accuracy and repeatability," said Ee Huei Sin, vice president, Keysight's General-Purpose Electronic Measurement Division. "With these innovations, including the world's first thermal vacuum compliant LAN sensor, Keysight sets a new standard in wireless and satellite testing."
U2049XA LAN Power Sensor
The U2049XA LAN power sensor achieves a number of industry firsts: 1) it is the world's first thermal vacuum compliant (TVAC) power sensor; and 2) it is the first power sensor to come with LAN/Power over Ethernet (PoE) connectivity.
U2049XA sensors with the thermal vacuum compliance option are subjected to temperature cycling in a vacuum chamber, and are created using components with minimal outgassing properties. The LAN-based sensor overcomes the cable length limitations associated with USB connectivity and is suitable for distances up to 100 meters. Together with best-in-class long term drift performance and a frequency range of 10 MHz to 33 GHz, the U2049XA is ideal for fault detection and long distance, remote monitoring of satellite systems.
U.S. Pricing and Additional Information
The new U2040 X-Series wide dynamic range power sensors are available worldwide. U.S. prices are as follows:
Model |
Description |
Frequency Range / Dynamic Range |
Price |
U2041XA |
USB wide dynamic range average power sensor |
10 MHz to 6 GHz / |
$3,500 |
U2042XA |
USB peak and average power sensor |
10 MHz to 6 GHz / |
$5,000 |
U2043XA |
USB wide dynamic range average power sensor |
10 MHz to 18 GHz / |
$4,500 |
U2044XA |
USB peak and average power sensor |
10 MHz to 18 GHz / |
$6,000 |
U2049XA |
LAN power sensor |
10 MHz to 33 GHz / |
$9,000 |
U2049XA (Option TVA) |
LAN power sensor (with thermal vacuum compliance) |
10 MHz to 33 GHz / |
$11,500 |
More information on the Keysight U2040 X-Series is available at www.keysight.com/find/WideDynamicSensor_pr. Images of the wide dynamic power sensors are available at www.keysight.com/find/WideDynamicSensor_images. A product video is available at www.keysight.com/find/WideDynamicSensor_video.
On Sept. 19, 2013, Agilent Technologies announced plans to separate into two publicly traded companies through a tax-free spinoff of its electronic measurement business. The new company, Keysight Technologies, began operating as a wholly owned subsidiary of Agilent on Aug. 1, 2014 with a full separation anticipated in early November 2014. Keysight is expected to trade on the NYSE under the symbol KEYS.
Keysight is a global electronic measurement technology and market leader helping to transform its customers' measurement experience through innovation in wireless, modular, and software solutions. Keysight provides electronic measurement instruments and systems and related software, software design tools and services used in the design, development, manufacture, installation, deployment and operation of electronic equipment. Information about Keysight is available at www.keysight.com.
Forward-Looking Statements
This news release contains forward-looking statements as defined in the Securities Exchange Act of 1934 and is subject to the safe harbors created therein. The forward-looking statements contained herein include, but are not limited to, information regarding Keysight's separation of the electronic measurement business; future revenues, earnings and profitability; the future demand for the company's products and services; and customer expectations. These forward-looking statements involve risks and uncertainties that could cause Keysight's results to differ materially from management's current expectations. Such risks and uncertainties include, but are not limited to, unforeseen changes in the strength of our customers' businesses; unforeseen changes in the demand for current and new products, technologies, and services; customer purchasing decisions and timing, and the risk that we are not able to realize the savings expected from integration and restructuring activities.
In addition, other risks that Keysight faces include those detailed in Keysight's filings with the Securities and Exchange Commission, including our Form 10, and amendments thereto. Forward-looking statements are based on the beliefs and assumptions of Keysight's management and on currently available information. Keysight undertakes no responsibility to publicly update or revise any forward-looking statement.
# # #
Contact:
Janet Smith, Americas
+1 970 679 5397
janet_smith@keysight.com
Twitter: @KeysightJSmith
Sarah Calnan, Europe
+44 (118) 927 5101
sarah_calnan@keysight.com
Connie Wong, Asia
+852 3197-7818
connie-ky_wong@keysight.com