SANTA ROSA, Calif., Aug. 8, 2014
Keysight Technologies, Inc. today announced two additions to its Signal Studio software suite of signal creation tools. The first is signal generation software for the IEEE 802.15.4g-based Wi-SUN standard. The second is support for LTE/LTE-Advanced uplink (UL) 2x2 MIMO with real-time Hybrid Automatic Repeat Request (HARQ). These new capabilities further ease the signal generation requirements for R&D and manufacturing engineers developing or testing the conformance of devices to the Wi-SUN and LTE/LTE-A standards.
"As a recognized industry leader in electronic measurement, Keysight is actively involved in the development, revision and implementation of emerging standards like Wi-SUN and LTE-Advanced," said Satish Dhanasekaran, marketing manager of Keysight's Microwave and Communications Division. "Keysight's new Signal Studio software capabilities complement our comprehensive portfolio of standards-based signal-generation and analysis solutions, and reaffirms our commitment to providing designers with the world-class solutions they need to move their standards-based designs forward."
N7610B Signal Studio
Keysight's new N7610B Signal Studio software generates Wi-SUN signals and supports the MR-FSK and MR-OFDM Wi-SUN modes. A fully coded advanced capability allows the software to easily make receiver conformance tests using Keysight signal generators (e.g., MXG/EXG, PSG/ESG or PXIe). For a more complete R&D and manufacturing solution, the N7610B can be used with Keysight signal analysis tools. Such functionality and flexibility make the N7610B well suited to support the needs of the emerging market for smart utility networks (e.g., smart grid) in Japan and those companies in the U.S. working on Wi-SUN-based solutions and products.
Based on the open global IEEE 802.15.4g-2012 standard, Wi-SUN is intended to advance and enable interoperable and reliable, cost-effective, low-power, wireless utility products for wireless smart utility networks and related applications. The 802.15.4g PHY carries multiple data rates in frequency bands from 450 MHz to 2.4 GHz and operates in three modes: 1) multi-rate multi-regional frequency shift keying (MR-FSK); 2) multi-rate orthogonal frequency division multiplexing (MR-OFDM); and 3) multi-rate multi-regional offset quadrature phase shift keying (MR-OQPSK).
N7624B/25B Signal Studio
LTE-A is a leading fourth-generation wireless communications technology defined in release ten and all follow-on releases of the 3GPP LTE standard. In the LTE eNB receiver conformance test section eight of release ten, a MIMO configuration with real-time HARQ capability on two antenna ports is required to test the physical uplink shared channel in transmissions with multipath fading propagation conditions.
Thanks to its support for uplink 2x2 MIMO with HARQ, the N7624B/25B Signal Studio for LTE/LTE-Advanced is well-equipped to meet this requirement. With this capability, the N7624B/25B becomes the industry's first LTE UL 2x2 MIMO with real-time HARQ signal generation solution, and Keysight becomes the sole provider of the industry's only complete LTE eNB receiver conformance test solution.
The N7624B/25B solution is ideal for base station R&D engineers working on LTE eNB receiver conformance testing to the 3GPP TS 36.141 standard. The software runs on either Keysight's PXB or X-Series signal generator. With the PXB, the 2x2 MIMO signal is configured directly on the PXB. An internal fader adds the propagation condition. The closed-loop feedback HARQ signal is generated by the eNB and sent to the PXB, where its baseband generator responds in real-time. Two RF signal generators then upconvert the signal for the PXB.
Keysight's X-Series signal generator with real-time baseband generator provides the same 2x2 MIMO signal generation capability and real-time response to the eNB HARQ signal as the PXB. This is accomplished by using two X-Series signal generators and an external fader.
U.S. Pricing and Availability
Keysight's new N7610B Signal Studio for Wi-SUN and N7624B/25B Signal Studio for LTE/LTE-Advanced with support for UL 2x2 MIMO with real-time HARQ are both now available. Pricing is as follows:
N7610B Signal Studio Option QFP Advanced MR-FSK
$2,800
Option RFP
Advanced MR-OFDM
$3,500
Signal Studio for LTE/LTE-AdvancedN7624B-WFP
Advanced LTE/LTE-Advanced FDD
real-time R9/R10 UL$9,687
N7624B-WFP
Advanced LTE/LTE-Advanced FDD
real-time R9/R10 UL$9,687
More information on Keysight's N7610B and N7624B/25B software is available at www.keysight.com/find/N7610B, www.keysight.com/find/N7624B and www.keysight.com/find/N7625B, respectively. Images of the software are available at www.keysight.com/find/SignalStudioLTE_images and www.keysight.com/find/N7610B_images.
On Sept. 19, 2013, Agilent Technologies announced plans to separate into two publicly traded companies through a tax-free spinoff of its electronic measurement business. The new company, Keysight Technologies, began operating as a wholly owned subsidiary of Agilent on Aug. 1, 2014 with a full separation anticipated in early November 2014. Keysight is expected to trade on the NYSE under the symbol KEYS.
Keysight is a global electronic measurement technology and market leader helping to transform its customers' measurement experience through innovation in wireless, modular, and software solutions. Keysight provides electronic measurement instruments and systems and related software, software design tools and services used in the design, development, manufacture, installation, deployment and operation of electronic equipment. Information about Keysight is available at www.keysight.com.
Forward-Looking Statements
This news release contains forward-looking statements as defined in the Securities Exchange Act of 1934 and is subject to the safe harbors created therein. The forward-looking statements contained herein include, but are not limited to, information regarding Keysight's separation of the electronic measurement business; future revenues, earnings and profitability; the future demand for the company's products and services; and customer expectations. These forward-looking statements involve risks and uncertainties that could cause Keysight's results to differ materially from management's current expectations. Such risks and uncertainties include, but are not limited to, unforeseen changes in the strength of our customers' businesses; unforeseen changes in the demand for current and new products, technologies, and services; customer purchasing decisions and timing, and the risk that we are not able to realize the savings expected from integration and restructuring activities.
In addition, other risks that Keysight faces include those detailed in Keysight's filings with the Securities and Exchange Commission, including our Form 10, and amendments thereto. Forward-looking statements are based on the beliefs and assumptions of Keysight's management and on currently available information. Keysight undertakes no responsibility to publicly update or revise any forward-looking statement.
# # #
Contact:
Janet Smith, Americas
+1 970 679 5397
[email protected]
Twitter: @KeysightJSmith
Sarah Calnan, Europe
+44 (118) 927 5101
[email protected]
Connie Wong, Asia
+852 3197-7818
[email protected]