SANTA CLARA, Calif., Jan. 8, 2014
Agilent Technologies Inc. (NYSE: A) today introduced the industry's first software for decoding USB 3.0 SuperSpeed Inter-Chip (SSIC) and MIPI Camera Serial Interface 3 (CSI-3) protocols on oscilloscopes. The new protocol decoders provide design and validation engineers with a fast, easy way to validate and debug their SSIC and CSI-3 interfaces.
SSIC is used for point-to-point communication between chips using the USB 3.0 protocol. The SSIC standard was developed by the USB-IF standards body, leveraging the MIPI(tm) Alliance MIPI M-PHY electrical layer to transfer USB 3.0 protocol. It allows USB 3.0 intellectual property and designs to be adopted into mobile applications.
The CSI-3 standard is the next-generation camera interface, developed by the MIPI Alliance to increase performance throughput and enable a greater feature set than the current CSI-2 standard. It also has better power-per-bit efficiency than the previous specification. The CSI-3 interface runs on top of the MIPI UniPro protocol layer as well as the MIPI M-PHY electrical layer.
Agilent's N8819A USB 3.0 SSIC and N8820A MIPI CSI-3 protocol decoders are designed to run on 90000A, 90000 X- and 90000 Q-Series oscilloscopes. They decode protocol packets for the SSIC v1.0 and MIPI CSI-3 v1.0 specifications, respectively. In addition to using the software for start-up debugging, R&D design and validation teams can use the software to snoop at traffic on the interfaces. They also provide accurate timing measurements associated with the protocols.
The software supports:
Engineers can use both protocol decoders on Infiniium 90000 Q-Series oscilloscopes, which deliver industry-leading, real-time bandwidth of up to 33 GHz on 4 channels, which makes them suitable for testing devices that use today's MIPI M-PHY data rates of 5.8 Gbps and for devices with data rates up to 11.6 Gbps, which is the next projected speed increase. With bandwidth upgradability to 63 GHz and the lowest noise and jitter measurement floor performance, the oscilloscopes ensure superior measurement accuracy and protect the user's investment when the next data-rate increase occurs
Used together with N2809A PrecisionProbe software, the protocol-decode software increases design margins and gives engineers increased confidence in their product performance. The N8805A USB 3.0 protocol decoder, N8808A UniPro protocol decoder and U7249B transmitter conformance software package are also available.
U.S. Pricing and Availability
The Agilent N8819A USB 3.0 SSIC and N8820A MIPI CSI-3 protocol decoders are available now for $3,500 and $3,000, respectively. Additional information is available at www.agilent.com/find/n8819a and www.agilent.com/find/n8820a. Software screen images are available at www.agilent.com/find/n8819a_images and www.agilent.com/find/n8820a_images.
Agilent's complete portfolio of oscilloscopes is available in a variety of form factors, from 20 MHz to 90 GHz, offering industry-leading specifications and powerful applications.
Agilent's Digital Test Standards Program
Agilent Digital Test Standards Program experts are involved in various international standards committees, including the Joint Electronic Devices Engineering Council, PCI-SIG, Video Electronics Standards Association, Serial ATA International Organization, Serial Attached SCSI (T10), USB-Implementers Forum, MIPI Alliance, Ethernet standards (IEEE 802.3), Optical Internetworking Forum and many others. Agilent's involvement in these standards groups enables the company to bring the right solutions to market when customers need them.
Agilent Technologies Inc. (NYSE: A) is the world's premier measurement company and a technology leader in chemical analysis, life sciences, diagnostics, electronics and communications. The company's 20,600 employees serve customers in more than 100 countries. Agilent had revenues of $6.8 billion in fiscal 2013. Information about Agilent is available at www.agilent.com.
On Sept. 19, 2013, Agilent announced plans to separate into two publicly traded companies through a tax-free spinoff of its electronic measurement business. The new company is named Keysight Technologies, Inc. The separation is expected to be completed in early November 2014.
# # #
Contact:
Janet Smith, Americas
+1 970 679 5397
janet_smith@agilent.com
Twitter: @JSmithAgilent
Sarah Calnan, Europe
+44 (118) 927 5101
sarah_calnan@agilent.com
Iris Ng, Asia
+852 31977979
iris-hw_ng@agilent.com