SANTA CLARA, Calif., May 8, 2014
Agilent Technologies Inc. (NYSE: A) today announced that GIT Japan Inc., a provider of advanced interface technologies between people and information, and a competence center for ultrawideband (UWB) chipset and module development, has selected Agilent EEsof EDA's Advanced Design System (ADS) electronic design automation platform for complete GaAs/GaN- and silicon-based RFIC/MMIC implementations.
"We successfully used the ADS front-to-back design flow for UWB power amplifier MMIC design in a WIN pHEMT process," said Shogo Ida, president and chief executive officer at GIT. "We also used it when expanding our portfolio to include silicon-based designs using IBM's high-performance SiGe BiCMOS technology. We chose ADS because it delivers proven RF circuit simulation, integrated EM solvers and RF-relevant backend support. It was key to our first-time-right tape-outs and enabled us to introduce unique products on time."
ADS is the most widely used platform for III-V MMIC design but also provides a complete RFIC design flow-including layout, enhanced foundry-certified PDKs, LVS and DRC-that is crucial for a successful implementation of wireless front-ends. The scalable front-to-back solution not only facilitates the job of the MMIC and RFIC designer from the beginning, but also directly integrates with other domains, such as RF modules and RF system-in-package (SiP) design.
Key ADS features like ADS Layout and Desktop DRC and LVS help simplify and speed the design flow. ADS Layout, for example, features an RFIC toolbar for easier, more efficient physical design and trace routing. Desktop DRC and LVS help verify and correct layouts against foundry DRC rules prior to tape out and catch errors early in the design cycle, all from the users' desktop. In addition, ADS' integrated 3D planar EM simulator Momentum combines full-wave and quasi-static EM solvers for simplified passive, interconnect and parasitic modeling.
"As a leader in the GaAs MMIC world, we have seen the popularity of the ADS platform for silicon-based RFIC design grow tremendously over the years," said Juergen Hartung, RFIC marketing manager for Agilent EEsof EDA. "Customers can now use these kits for a variety of RF CMOS, RF SOI and SiGe BiCMOS technologies to enjoy full back-end support that includes schematic-driven layout creation, layout-versus-schematic check, and integrated 3D planar electromagnetic and 3D-FEM simulators."
About Advanced Design System
The leading electronic design automation software for RF, microwave and signal integrity applications, ADS pioneers the most innovative and commercially successful technologies, such as X-parameters* and 3-D electromagnetic simulators. ADS 2014 addresses the most challenging design complexity and integration needs of leading-edge commercial wireless and aerospace/defense companies, by enabling them to design multi-technology RF system-in-package modules and perform complex electromagnetic simulations-all with greater ease and speed. More information is available at www.agilent.com/find/eesof-ads.
About Agilent EEsof EDA Software
Agilent EEsof EDA is the leading supplier of electronic design automation software for microwave, RF, high-frequency, high-speed digital, RF system, electronic system level, circuit, 3-D electromagnetic, physical design and device-modeling applications. More information is available at www.agilent.com/find/eesof.
Agilent Technologies Inc. (NYSE: A) is the world's premier measurement company and a technology leader in chemical analysis, life sciences, diagnostics, electronics and communications. The company's 20,600 employees serve customers in more than 100 countries. Agilent had revenues of $6.8 billion in fiscal 2013. Information about Agilent is available at www.agilent.com.
On Sept. 19, 2013, Agilent announced plans to separate into two publicly traded companies through a tax-free spinoff of its electronic measurement business. The new company is named Keysight Technologies, Inc. The separation is expected to be completed in early November 2014.
# # #
*X-parameters is a trademark and registered trademark of Agilent Technologies in the U.S., EU, JP, and elsewhere. The X-parameters format and underlying equations are open and documented. For more information, visit www.agilent.com/find/eesof-x-parameters-info.
Contact:
Janet Smith, Americas
+1 970 679 5397
[email protected]
Twitter: @JSmithAgilent
Sarah Calnan, Europe
+44 (118) 927 5101
[email protected]
Connie Wong, Asia
+852 3197-7818
[email protected]