SANTA CLARA, Calif., May 8, 2014
Agilent Technologies Inc. (NYSE: A) today announced that its T3111S">T3111S NFC Conformance Test System has been validated for testing of NFC Forum Logical Link Protocol (LLCP) and Simple NDEF Exchange (SNEP) Protocol. The T3111S is the only test platform combining validated NFC Forum analog RF, digital protocol, LLCP and SNEP testing in one integrated system.
LLCP and SNEP enable peer-to-peer communication between smartphones and other mobile devices using Near Field Communication (NFC). They enable users to intuitively pass URLs and contact details, and they trigger other mobile protocols to exchange photos and other large files. LLCP defines an OSI layer-2 protocol to support peer-to-peer communication between two NFC-enabled devices. SNEP allows application messages in NFC Data Exchange Format (NDEF) to be exchanged between devices.
The Agilent T3111S was used to certify the first NFC Forum devices in 2012. Used in test laboratories worldwide, the Agilent NFC Conformance Test System has enabled an ever-growing number of devices from many vendors to be successfully certified. From digital protocol to analog RF, and now with LLCP and SNEP, the T3111S system capabilities have expanded with each enhancement to NFC Forum certification.
In addition, the Agilent T3111S Test System delivers a comprehensive array of other significant automated test suites, including EMVTM Level 1 analog RF; EMV Level 1 digital protocol; and ISO 14443, 18092, 15693 and 18000-3 testing methods.
"With this new approval from the NFC Forum, we are delighted that the T3111S has become the first integrated test system with validation in each area of NFC Forum conformance testing," said Joe DePond, vice president and general manager of Agilent's Mobile Broadband Operation. "We are committed to supporting NFC testing across the entire R&D lifecycle."
"Agilent has demonstrated its commitment to NFC, both as a valued partner to the NFC Forum Certification Program and as a Forum member," said Paula Hunter, executive director of the NFC Forum. "By making it possible for manufacturers to more thoroughly test their NFC devices, the T3111S NFC Conformance Test System will help to broaden the reach and impact of our certification program."
The NFC Forum Certification Program gives device manufacturers a means of establishing their products' compliance with the NFC Forum's technical specifications. The program offers increased assurance that NFC Forum-certified products are interoperable with other NFC Forum-certified products. It also supports consistency in the behavior of NFC devices by confirming that products conform to NFC Forum specifications. Agilent has consistently supported the NFC Forum's program.
Additional Information
Information about Agilent T3111S NFC Conformance Test System is available at www.agilent.com/find/T3111S. The T3111S is available now; pricing depends on system configuration. A quote is available upon request from Agilent.
T3111S images are available at www.agilent.com/find/T3111S_images.
Agilent's LTE design and test portfolio is at www.agilent.com/find/LTE.
Agilent Technologies Inc. (NYSE: A) is the world's premier measurement company and a technology leader in chemical analysis, life sciences, diagnostics, electronics, and communications. The company's 20,600 employees serve customers in more than 100 countries. Agilent had revenues of $6.8 billion in fiscal 2013. Information about Agilent is available at www.agilent.com.
On Sept. 19, 2013, Agilent announced plans to separate into two publicly traded companies through a tax-free spinoff of its electronic measurement business. The new company is named Keysight Technologies, Inc. The separation is expected to be completed in early November 2014.
# # #
Contact:
Janet Smith, Americas
+1 970 679 5397
janet_smith@agilent.com
Twitter: @JSmithAgilent
Sarah Calnan, Europe
+44 (118) 927 5101
sarah_calnan@agilent.com
Connie Wong, Asia
+852 3197-7818
connie-ky_wong@agilent.com