Keysight Technologies Introduces First MHL 3 Source Compliance Test Software

  
  

SANTA ROSA, Calif., Dec. 9, 2014

Keysight Technologies, Inc. (NYSE: KEYS) today introduced compliance test software for the latest Mobile High-Definition Link (MHL) specification. The MHL 3 source compliance test software allows engineers to test their MHL 3 transmitters the same way they are tested at official authorized MHL compliance test centers using Keysight Infiniium oscilloscopes.

Leading manufacturers are implementing MHL technology in consumer products such as tablets, mobile phones and automotive audiovisual accessories, which requires them to pay close attention to device interoperability. The MHL 3 specification, published in August 2013, offers a significant increase in bandwidth (up to 6 Gbps) to support higher resolution and a new bidirectional high-speed communication path between the portable device and a display.

Keysight's N6460B transmitter compliance solution builds on its MHL 2 transmitter compliance test software that is also currently used worldwide in MHL authorized test centers. The new software offers test capabilities now required for MHL 3 transmitters, such as a dedicated TMDS lane and new functionality in the CBus, referred to now as eCBus, that includes forward and reverse transmission validation.

"Consumers want to be confident that the MHL products they purchase will deliver the performance and interoperability they desire, ensuring that devices work together effortlessly," said Solomon Langley, general manager, Simplay Labs. "Keysight's development engineers have worked on the N6460B compliance software with our validation teams on measurement algorithms to optimize accuracy and usability. Keysight is an important piece of our interoperability program, and we look forward to continuing to work with them as we move to future versions of the MHL specification."

The Keysight MHL 3 compliance software includes new features along with test suites for all previous versions of MHL, which are required to validate interoperability of MHL 3 devices. The software feature set includes:

  • MHL 1, MHL 2 and MHL 3 test suites
  • Cable model and equalizer setup for complete control in what-if analysis as well as standard compliance testing
  • User-defined mask setup to suit individual company goals as well as standard masks required in compliance testing
  • DUT automation control for MHL 3 unattended testing using Simplay Labs test accessories
  • Saved waveform analysis to import waveforms for remote support or offline analysis
  • User comments for in-depth details in test reports
  • Calibration test suites for MHL TMDS receiver test as well as source device eCBus receiver testing

Keysight's MHL source compliance testing solution includes:

Full MHL 3 link analysis requires Keysight's receiver cable compliance testing solutions, including Keysight E4887A TMDS signal generators, the M8190A arbitrary waveform generator and N5990A factory automation software. The receiver compliance solution is complemented by products from Keysight's solutions partner BitifEye. BitifEye products include test fixture and an MHL upgrade of BitifEye's frame generator software.

Additional information about Keysight MHL 3 transmitter compliance test software is available at www.keysight.com/find/N6460B. Additional information about Keysight's MHL receiver compliance test software is available at www.keysight.com/find/mhl.

Keysight's complete portfolio of oscilloscopes is available in a variety of form factors, from 20 MHz to 90 GHz, offering industry-leading specifications and powerful applications.

U.S. Pricing and Availability

The Keysight MHL 3 transmitter compliance test application is available now for $8000. The Keysight MHL 3 receiver compliance test application is available now for $14,000.

Keysight's Digital Test Standards Program

Keysight Digital Test Standards Program experts are involved in various international standards committees, including the SD Association, Joint Electronic Devices Engineering Council, PCI-SIG®, Video Electronics Standards Association, Serial ATA International Organization, Serial Attached SCSI (T10), USB-Implementers Forum, MIPI Alliance, Ethernet standards (IEEE 802.3), Optical Internetworking Forum and many others. Keysight's involvement in these standards groups enables the company to bring the right solutions to market when customers need them.
About Keysight Technologies

Keysight Technologies (NYSE:KEYS) is a global electronic measurement technology and market leader helping to transform its customers' measurement experience through innovations in wireless, modular, and software solutions. Keysight's electronic measurement instruments, systems, software and services are used in the design, development, manufacture, installation, deployment and operation of electronic equipment. The business had revenues of $2.9 billion in fiscal year 2014. Information about Keysight is available at www.keysight.com.

# # #

PCI SIG® is a US registered trademark and/or service mark of PCI-SIG. MIPI is a licensed trademark of MIPI, Inc. in the U.S. and other jurisdictions.

Contact:

Janet Smith, Americas
+1 970 679 5397
[email protected]
Twitter: @KeysightJSmith

Sarah Calnan, Europe
+44 (118) 927 5101
[email protected]

Connie Wong, Asia
+852 3197-7818
[email protected]