SANTA CLARA, Calif., July 9, 2014
Agilent Technologies Inc. (NYSE: A) today announced the industry's most accurate test solution for characterizing USB 3.1 receivers. Using the Agilent USB 3.1 receiver test set, design and test engineers in the semiconductor and computer industry can now accurately characterize and verify USB 3.1 receiver ports in ASICs and chipsets.
USB interfaces are commonly used in today's PCs, tablets, mobile phones and external storage devices. The new USB 3.1 specification was released by the USB Implementers Forum in 2013, and the first USB 3.1 10-Gb/s-capable products are expected to reach the market in 2014. The USB 3.1 specification more than doubles possible throughput compared with the USB 3.0 specification. This throughput improvement was achieved by doubling the physical data rate from 5 to 10 Gb/s and by changing the coding scheme from 8-bit/10-bit to 128-bit/132-bit, which requires significantly less overhead.
"Agilent's new USB 3.1 receiver test solution fills a critical need for ASIC and chipset designers needing to quickly deliver the next generation of USB-enabled devices," said Juergen Beck, vice president and general manager of Agilent's Digital & Photonic Test Division. "With our expertise in accurate receiver tolerance testing, we continue to help R&D teams efficiently release robust, next-generation chipsets for the semiconductor and computer industry."
R&D and test engineers who design and test USB 3.1 chipsets are facing new challenges. For receiver test, the doubled physical data rate means the margins for signal integrity are tighter. To ensure proper operation, the receiver must tolerate a mix of different jitter types. Three-tap de-emphasis is required to compensate for the losses of the channel. And finally, the analyzer must be able to filter 128-bit/132-bit coded skip-ordered sets with variable length during error counting.
Benefits of the Agilent USB 3.1 receiver test solution include:
The Agilent USB 3.1 receiver test solution consists of either:
U.S. Pricing and Availability
The price for the J-BERT M8020A high-performance BERT starts at $122,200 for a one-channel, 16-Gb/s high-performance BERT with built-in clock recovery.
The upgradeable J-BERT N4903B (the new option for analyzing 128b/132b-coded patterns) is priced at $12,500. The J-BERT requires software version 7.60 or later.
All products are available today.
More information about Agilent's USB 3 receiver test solutions is available at www.agilent.com/find/usb3_receiver_test.
Agilent offers a wide selection of high-speed digital solutions including essential tools to pinpoint problems, optimize devices and deliver results for design and simulation. Agilent will present a webcast about USB test challenges on July 16.
Agilent Technologies Inc. (NYSE: A) is the world's premier measurement company and a technology leader in chemical analysis, life sciences, diagnostics, electronics and communications. The company's 20,600 employees serve customers in more than 100 countries. Agilent had revenues of $6.8 billion in fiscal 2013. Information about Agilent is available at www.agilent.com.
On Sept. 19, 2013, Agilent announced plans to separate into two publicly traded companies through a tax-free spinoff of its electronic measurement business. The new company is named Keysight Technologies, Inc. The separation is expected to be completed in early November 2014.
# # #
Contact:
Janet Smith, Americas
+1 970 679 5397
[email protected]
Twitter: @JSmithAgilent
Sarah Calnan, Europe
+44 (118) 927 5101
[email protected]
Connie Wong, Asia
+852 3197-7818
[email protected]