SANTA ROSA, Calif., Oct. 10, 2014
Keysight Technologies, Inc. today announced the availability of its Method of Implementation (MOI) document for USB 2.0 connector and cable assembly compliance testing using the ENA Series network analyzer's enhanced time domain analysis option (E5071C-TDR).
Developed in the mid-1990s, the USB standard features a number of variants including SuperSpeed USB, also known as USB 3.0, which supports a 5 Gbps transfer rate and offers up to a 10 times performance increase over its predecessor USB 2.0 (Hi-Speed USB). While USB 3.0 has been widely adopted, USB 2.0 remains popular for car navigation systems and other applications where a 480 Mbps or less transfer rate is just enough. Here, cable assemblies are considered captive if they are provided with a vendor-specific connect means (hardwired or custom detachable) to the peripheral. To ensure all such connectors and cable assemblies comply with the USB 2.0 standard, they must be tested in accordance with the specification.
While Keysight already offers a MOI for USB 3.0 connector and cable assembly compliance tests, support for USB 2.0 has now been added to the mix. The result is a complete USB solution that provides engineers with a measurement guide of procedures that supports compliance testing to both the USB 2.0 and 3.0 standards. Using the MOI, state files and calibration kit files, cable and connector manufacturers and product integrators can now more efficiently perform compliance tests to the USB standard with the E5071C-TDR.
"Keysight's MOIs cover a range of diverse high-speed digital applications like HDMI and high-speed Ethernet," said Akira Nukiyama, vice president and general manager, Keysight's Component Test Division. "The addition of USB 2.0 support further expands this list and reinforces our commitment to ensuring customers have the tools they need to address any high-speed measurement challenges that might arise."
The USB MOI for use with the E5071C-TDR is available at www.keysight.com/find/ena-tdr_compliance. Additional information on MOI for connector and cable assembly compliance test is available at www.keysight.com/find/ena-tdr_USB2-cabcon. An image of the new ENA Series network analyzer's enhanced time domain analysis option is available at www.keysight.com/find/e5071C_TDR_USB2_MOI_images.
About ENA Option TDR
The E5071C ENA-TDR is an application embedded in the ENA network analyzer that provides a one-box solution for high-speed serial interconnect analysis. The software delivers three breakthroughs for signal integrity design and verification: simple and intuitive operation, fast and accurate measurements simultaneously in the time domain (TDR/TDT) and frequency domain (S-parameter), and ESD robustness for reduction of maintenance cost.
On Sept. 19, 2013, Agilent Technologies announced plans to separate into two publicly traded companies through a tax-free spinoff of its electronic measurement business. The new company, Keysight Technologies, began operating as a wholly owned subsidiary of Agilent on Aug. 1, 2014 with a full separation anticipated in early November 2014. Keysight is expected to trade on the NYSE under the symbol KEYS.
Keysight is a global electronic measurement technology and market leader helping to transform its customers' measurement experience through innovation in wireless, modular, and software solutions. Keysight provides electronic measurement instruments and systems and related software, software design tools and services used in the design, development, manufacture, installation, deployment and operation of electronic equipment. Information about Keysight is available at www.keysight.com.
Forward-Looking Statements
This news release contains forward-looking statements as defined in the Securities Exchange Act of 1934 and is subject to the safe harbors created therein. The forward-looking statements contained herein include, but are not limited to, information regarding Keysight's separation of the electronic measurement business; future revenues, earnings and profitability; the future demand for the company's products and services; and customer expectations. These forward-looking statements involve risks and uncertainties that could cause Keysight's results to differ materially from management's current expectations. Such risks and uncertainties include, but are not limited to, unforeseen changes in the strength of our customers' businesses; unforeseen changes in the demand for current and new products, technologies, and services; customer purchasing decisions and timing, and the risk that we are not able to realize the savings expected from integration and restructuring activities.
In addition, other risks that Keysight faces include those detailed in Keysight's filings with the Securities and Exchange Commission, including our Form 10, and amendments thereto. Forward-looking statements are based on the beliefs and assumptions of Keysight's management and on currently available information. Keysight undertakes no responsibility to publicly update or revise any forward-looking statement.
# # #
Contact:
Janet Smith, Americas
+1 970 679 5397
[email protected]
Twitter: @KeysightJSmith
Sarah Calnan, Europe
+44 (118) 927 5101
[email protected]
Connie Wong, Asia
+852 3197-7818
[email protected]