Keysight Technologies Introduces 65-GSa/s High-Speed Arbitrary Waveform Generator

  
  

SANTA ROSA, Calif., Sept. 10, 2014

Keysight Technologies, Inc. today added a 65-GSa/s, 20-GHz modular instrument to its portfolio of arbitrary waveform generators. The new high-speed, wide-bandwidth M8195A arbitrary waveform generator allows engineers to generate digital, multilevel (e.g. PAM4, MIPI C-PHY) signal scenarios and test their electrical and optical links with complex modulated signals up to 32 GBaud and beyond. This makes the M8195A the most versatile signal generator in the industry.

The instantaneous bandwidth from DC to 20 GHz allows researchers to create extremely short, yet precise pulses. Developers of radar, electronic warfare, satellite and wireless applications can use the M8195A AWG to create wideband signals up to 20 GHz. The instrument delivers high sample rate and wide bandwidth in combination with industry-leading port density. This unique functionality allows engineers to make reliable, repeatable measurements when they are working on binary and multilevel, multichannel digital interfaces as well as coherent optical and wideband communication applications.

The M8195A uses out-of-the box and in-situ calibration and signal predistortion methods to generate exceptionally clean signals — even at the highest data rates. Engineers also can use these techniques to embed or de-embed the channel between the generator and the device under test. The implementation in hardware allows change of parameters at runtime.

With up to 16 GSamples of waveform memory, the M8195A allows designers to create long and highly realistic signal scenarios. Multiple M8195A modules can be combined in a system with up to 16 fully synchronous channels in a single 5-slot AXIe chassis.

"The M8195A uses proprietary ASIC technology to deliver a combination of the fastest speed, widest bandwidth and highest port density," said Juergen Beck, vice president and general manager of Keysight's digital and photonic test business. "This enables customers to economically test their multichannel, high-speed designs to the limit of required functionality."

The M8195A arbitrary waveform generator helps engineers to:

  • Generate four channels of multilevel signals (e.g PAM4) with programmable distortions and jitter up to 32 Gbaud.
  • Generate two pairs of complex modulated baseband signals (four channels) for coherent optical applications up to 32 GBaud and beyond.

The M8195A offers:

  • A maximum sample rate of 65-GSa/s with 20 GHz of analog bandwidth on up to four precisely aligned channels per 1-slot AXIe module simultaneously.
  • Up to 2 Vpp differential output voltage and adjustable DC offset in a -1 to 3.3 V window.
  • The ability to build realistic scenarios with up to 16 GSa of waveform memory.

The M8195A runs on an AXIe modular system designed for high-performance instrumentation and can be used with a 2-slot or 5-slot chassis.

Additional Information

Shipments for the M8195A arbitrary waveform generator begin Sept. 30 with an entry price of $100,000.

Additional information is available at www.keysight.com/find/M8195A. High-resolution images are available at www.keysight.com/find/M8195_images.


About Keysight Technologies

On Sept. 19, 2013, Agilent Technologies announced plans to separate into two publicly traded companies through a tax-free spinoff of its electronic measurement business. The new company, Keysight Technologies, began operating as a wholly owned subsidiary of Agilent on Aug. 1, 2014 with a full separation anticipated in early November 2014. Keysight is expected to trade on the NYSE under the symbol KEYS.

Keysight is a global electronic measurement technology and market leader helping to transform its customers' measurement experience through innovation in wireless, modular, and software solutions. Keysight provides electronic measurement instruments and systems and related software, software design tools and services used in the design, development, manufacture, installation, deployment and operation of electronic equipment. Information about Keysight is available at www.keysight.com.

Forward-Looking Statements

This news release contains forward-looking statements as defined in the Securities Exchange Act of 1934 and is subject to the safe harbors created therein. The forward-looking statements contained herein include, but are not limited to, information regarding Keysight's separation of the electronic measurement business; future revenues, earnings and profitability; the future demand for the company's products and services; and customer expectations. These forward-looking statements involve risks and uncertainties that could cause Keysight's results to differ materially from management's current expectations. Such risks and uncertainties include, but are not limited to, unforeseen changes in the strength of our customers' businesses; unforeseen changes in the demand for current and new products, technologies, and services; customer purchasing decisions and timing, and the risk that we are not able to realize the savings expected from integration and restructuring activities.

In addition, other risks that Keysight faces include those detailed in Keysight's filings with the Securities and Exchange Commission, including our Form 10, and amendments thereto. Forward-looking statements are based on the beliefs and assumptions of Keysight's management and on currently available information. Keysight undertakes no responsibility to publicly update or revise any forward-looking statement.

# # #

Contact:

Janet Smith, Americas
+1 970 679 5397
[email protected]
Twitter: @KeysightJSmith

Sarah Calnan, Europe
+44 (118) 927 5101
[email protected]

Connie Wong, Asia
+852 3197-7818
[email protected]