Agilent Technologies Offers First User-Extensible Recorder Application for Real-Time Spectrum Analyzers

  
  

SANTA CLARA, Calif., April 15, 2014

Agilent Technologies Inc. (NYSE: A) today announced the availability of the option RTR, the industry's first real-time spectrum recorder and analyzer application example for real-time spectrum analyzers (RTSAs).

Option RTR enhances the RTSA capabilities currently available for the Agilent PXA and MXA signal analyzers. Option RTR enables engineers to record, analyze and play back signal spectrum density data for detecting and analyzing signal anomalies, and for viewing the evolution of signals and spectrum density over time. Option RTR includes the application, the application source code for user extensibility, and MATLAB software to extend the application's capabilities as needed to meet current and future testing needs.

Option RTR addresses many important signal analysis challenges, including:

  • Detecting and analyzing signal anomalies, such as hard-to-detect edge cases;
  • Identifying the highest power signal received during a period of interest by placing density and density envelope cursors;
  • Studying a signal spectrum in which low-powered signals are followed by high-powered signals at the same frequency; and
  • Studying a spectrum in which multiple signal bursts occur at different frequencies at different times, and the relative times and the number of occurrences of the signals at each frequency is important.

By detecting, analyzing and resolving signal anomalies early, engineers are able to accelerate time-to-insight and time-to-market of RF designs such as radar, defense and wireless communication devices.

"Option RTR provides meaningful real-time recorder and playback capabilities, which allows our customers to solve difficult signal analysis challenges," said Bob Witte, vice president, Agilent's Technology Leadership Organization. "In addition, if a project has signal analysis requirements beyond the out-of-the-box application capabilities, customers can immediately customize and extend the solution to meet their unique testing needs."

Option RTR can be purchased with an Agilent N9030A PXA or N9020A MXA with real-time spectrum analyzer option RT1 or RT2. Option RT1 or RT2 and option RTR can be added later as an upgrade to the N9030A or N9020A.

Availability

For more information about option RTR, go to www.agilent.com/find/RTR. More information about the real-time spectrum analyzer options is available at www.agilent.com/find/RTSA. Information about the N9020A MXA Signal Analyzer, 10 Hz to 26.5 GHz, is available at www.agilent.com/find/MXA. Information about the N9030A PXA Signal Analyzer, 3 Hz to 50 GHz, is available at www.agilent.com/find/PXA.

About MATLAB Software Available from Agilent

Agilent is the first and only test and measurement company today that sells and supports MATLAB software with its instruments, offering a complete hardware and software test solution to engineers.

In addition to including MATLAB software with Agilent instrument option RTR, MATLAB software is available as a software option with other Agilent instruments. For information about MATLAB software for use with Agilent signal generators, signal analyzers, arbitrary waveform generators, network analyzers, and PXI and AXIe controllers go to www.agilent.com/find/matlab. For information about MATLAB software for use with Agilent Infiniium and InfiniiVision oscilloscopes go to www.agilent.com/find/matlab_oscilloscopes.


About Agilent Technologies

Agilent Technologies Inc. (NYSE: A) is the world's premier measurement company and a technology leader in chemical analysis, life sciences, diagnostics, electronics and communications. The company's 20,600 employees serve customers in more than 100 countries. Agilent had revenues of $6.8 billion in fiscal 2013. Information about Agilent is available at www.agilent.com.

On Sept. 19, 2013, Agilent announced plans to separate into two publicly traded companies through a tax-free spinoff of its electronic measurement business. The new company is named Keysight Technologies, Inc. The separation is expected to be completed in early November 2014.

# # #

Contact:

Janet Smith, Americas
+1 970 679 5397
[email protected]
Twitter: @JSmithAgilent

Sarah Calnan, Europe
+44 (118) 927 5101
[email protected]

Connie Wong, Asia
+852 3197-7818
[email protected]