SANTA CLARA, Calif., Jan. 16, 2014
Agilent Technologies Inc. (NYSE: A) today introduced a debugging tool that helps DDR memory designers perform precompliance tests, discover the root cause of compliance failures, and maximize design margins. The tool allows designers to easily navigate to areas of interest for further analysis and collect and analyze statistical data. The DDR3 and LPDDR3 debug tool runs on Infiniium 9000A, 90000A, 90000 X- and 90000 Q-Series oscilloscopes.
For engineers who work in the computer, server and mobile device industries, the new tool makes it easier to debug DDR memory devices. It includes statistical analysis on DDR3 and LPDDR3 timing measurements per the JEDEC standard as well as markers to indicate measurement points.
The U7231B-3NL DDR3 and LPDDR3 debug tool works on saved waveform files from Agilent oscilloscopes. It locates the start and end of read and write bursts found in the trace to enable quick timing measurements. Engineers can then navigate easily to problem areas to perform further analysis and margin tests.
"Our new DDR debug tool addresses the growing need for memory design engineers to debug their memory systems quickly and more efficiently," said Jay Alexander, vice president and general manager of Agilent's Oscilloscope and Protocol Division. "This tool complements Agilent's existing DDR compliance test software to provide debugging capability in a high-speed memory testing environment."
Additional information about Agilent's DDR3 and LPDDR3 compliance test solution can be found at www.agilent.com/find/u7231b. Product images are available at www.agilent.com/find/U7231b3NL_images.
Agilent's complete oscilloscope portfolio includes instruments with a variety of form factors and with bandwidths from 20 MHz to 90 GHz.
U.S. Pricing and Availability
The Agilent U7231B-3NL DDR3 and LPDDR3 debug tool is available now as an option for the DDR3 and LPDDR3 compliance test application software. The debug tool is priced at $2,000. Debug tools for other DDR technologies will be available soon.
Agilent Technologies Inc. (NYSE: A) is the world's premier measurement company and a technology leader in chemical analysis, life sciences, diagnostics, electronics and communications. The company's 20,600 employees serve customers in more than 100 countries. Agilent had revenues of $6.8 billion in fiscal 2013. Information about Agilent is available at www.agilent.com.
On Sept. 19, 2013, Agilent announced plans to separate into two publicly traded companies through a tax-free spinoff of its electronic measurement business. The new company is named Keysight Technologies, Inc. The separation is expected to be completed in early November 2014.
# # #
Contact:
Janet Smith, Americas
+1 970 679 5397
janet_smith@agilent.com
Twitter: @JSmithAgilent
Sarah Calnan, Europe
+44 (118) 927 5101
sarah_calnan@agilent.com
Iris Ng, Asia
+852 31977979
iris-hw_ng@agilent.com