SANTA ROSA, Calif., Dec. 17, 2014
Keysight Technologies, Inc. (NYSE: KEYS) today announced comprehensive pulsed radar analysis software. The new 89600 VSA software's pulse analysis option (BHQ) is used in radar and electronic counter measure applications for capturing and analyzing threats and jamming responses.
The software option gives R&D engineers the flexibility to define unique pulse characteristics and analyze them in the time and frequency domains. The software also provides tabular statistical reports summarizing the critical pulse parameters that are of interest to system designers.
Used in conjunction with the recently introduced UXA X-Series signal analyzer, designers can make pulse measurements up to 510 MHz analysis bandwidth – the widest RF analysis bandwidth available today. The analyzer also has excellent phase noise and dynamic range specifications.
For designers using the Infiniium oscilloscopes or the M9703A wideband digitizer to achieve even wider bandwidths, a new segmented memory capture feature can reduce memory consumption. By recording only pulses, with minimal recording of off-pulse time, segmented memory capture makes a longer recording period possible. This means that these instruments can now gather a greater amount of data, allowing designers to characterize complex pulse signals with more confidence than ever before.
"In-depth pulsed radar analysis capabilities are essential for system design in aerospace, defense and electronic warfare applications, where mission criticality is at stake," said Satish Dhanasekaran, marketing manager, Keysight's Microwave & Communications Division. "The 89600 VSA software is just one example of the many ways that Keysight applies years of test and measurement expertise to the task of putting powerful and evolving software tools into the hands of the designers. This allows them to gain deeper and unique insight into their engineering challenges."
About 89600 VSA Software
Keysight's industry-leading 89600 VSA software is a comprehensive set of tools for signal demodulation and vector signal analysis. It is widely used in cellular, wireless-connectivity, aerospace and defense applications. 89600 VSA software allows users to explore virtually every facet of a signal and optimize their most advanced designs. The software supports connectivity to over 40 different Keysight hardware products.
U.S. Pricing and Availability
The new pulse analysis option (BHQ) for the 89600 VSA software is priced at $5,000 and is available today.
N9051B X-Series pulse measurement software, Option 5FP, and the N9051A to N9051B upgrade are available for purchase today and are priced as follows:
More information on the 89600 VSA software and its new analysis capability is available at www.keysight.com/find/vsa_enhancements. More information on the N9051B is available at www.keysight.com/find/N9051B.
Free 30-day software trials are available by clicking on the Trials and Licenses tab at www.keysight.com/find/89600 or www.keysight.com/find/N9051B.
Images of the 89600 VSA and N9051B software analysis capabilities are available at www.keysight.com/find/89600vsa_images.
More information about Keysight's software is available www.keysight.com/find/software, including a link to Keysight's 2014 Market Leadership Software Instrumentation award from Frost & Sullivan.Keysight Technologies (NYSE:KEYS) is a global electronic measurement technology and market leader helping to transform its customers' measurement experience through innovations in wireless, modular, and software solutions. Keysight's electronic measurement instruments, systems, software and services are used in the design, development, manufacture, installation, deployment and operation of electronic equipment. The business had revenues of $2.9 billion in fiscal year 2014. Information about Keysight is available at www.keysight.com.
# # #
Contact:
Janet Smith, Americas
+1 970 679 5397
[email protected]
Twitter: @KeysightJSmith
Sarah Calnan, Europe
+44 (118) 927 5101
[email protected]
Connie Wong, Asia
+852 3197-7818
[email protected]