SANTA CLARA, Calif., May 21, 2014
Agilent Technologies Inc. (NYSE: A) today introduced a new averager real-time processing function for its PCIe digitizer family.
Averaging selected out of the growing range of real-time applications.
Averaging signals reduces random noise effects, which improves the signal-to-noise ratio and increases resolution and dynamic range. The fast sampling rate of up to 3.2 GS/s is achieved with a single trigger and acquisition, and does not require the use of equivalent-time sampling techniques. With averaging up to 520,000 triggers per record and a self-trigger mode to effectively minimize synchronous pattern noise within the application, the averager functionality adds a layer to the ever-growing versatility of the Agilent PCIe digitizer family.
The average capabilities, together with the recently announced peak detection and digitizer real-time functions, provide Agilent customers with a complete and flexible toolbox to achieve the best analysis possible for their applications' requirements. The software driver included with the digitizer allows the application to easily switch between signal processing functions.
"With our frequent release of additional real-time processing, customers can benefit from ever-increasing measurement throughputs," said Didier Lavanchy, operations manager for Agilent's high-speed digitizers. "And by using the U5340A FPGA development kit, customers can rapidly address their development requirements."
The averager option (-AVG) is available now on the 8-bit U5309A and 12-bit U5303A PCIe high-speed digitizers. Please contact [email protected] for more information.
The Agilent U5303A PCIe 12-bit High-Speed Digitizer recently won ECN magazine's Impact Award for Boards and Modules. More information is available at www.ecnmag.com/news/2014/05/ecn-impact-awards-honors-outstanding-achievement-design-engineering.
Information about product configuration is available at www.agilent.com/find/U5309A and www.agilent.com/find/U5303A.
High-resolution images are available at www.agilent.com/find/Averager_PCIe_Digitizers_images.
About Agilent High-Speed Digitizers
Agilent high-speed digitizers are the result of more than 300 years of cumulative research and development experience in analog-to-digital conversion technology. This ensures the ability to achieve the most effective and reliable analog-to-digital conversion at high resolution and fast sampling rates. Information on the technology and its applications is available at high-speed-digitizer.tm.agilent.com.
Agilent Technologies Inc. (NYSE: A) is the world's premier measurement company and a technology leader in chemical analysis, life sciences, diagnostics, electronics and communications. The company's 20,600 employees serve customers in more than 100 countries. Agilent had revenues of $6.8 billion in fiscal 2013. Information about Agilent is available at www.agilent.com.
On Sept. 19, 2013, Agilent announced plans to separate into two publicly traded companies through a tax-free spinoff of its electronic measurement business. The new company is named Keysight Technologies, Inc. The separation is expected to be completed in early November 2014.
# # #
PCIe and PCI EXPRESS are registered trademarks and/or service marks of PCI-SIG.
Contact:
Janet Smith, Americas
+1 970 679 5397
[email protected]
Twitter: @JSmithAgilent
Sarah Calnan, Europe
+44 (118) 927 5101
[email protected]
Connie Wong, Asia
+852 3197-7818
[email protected]