SANTA CLARA, Calif. Jan. 22, 2014
Agilent Technologies Inc. (NYSE: A) today announced the E8486A waveguide power sensor. Designed with a WR-12 flange connector, the E8486A makes precise and accurate power measurements in the E-band spectrum of 60 to 90 GHz, making the sensor the ideal solution to meet the rapid demand in E-band telecommunication applications.
The E8486A comes with an 80 dB dynamic range option, allowing the sensor to measure from -60 dBm to +20 dBm instead of the standard -30 dBm to +20 dBm range. With the expanded dynamic range, the E8486 continues to be highly accurate even when measuring low-level signals, making it possible to measure power at the receiver side of point-to-point transceiver modules in addition to the module's output power.
Like all Agilent waveguide power sensors, the E8486A offers high reliability and low loss. For easy calibration, the E8486A incorporates a 50 MHz calibration port to eliminate the uncertainties due to temperature changes and the variance in making measurements with different meter and sensor combinations. The E8486A also offers excellent SWR of 1.06, minimizing any measurement uncertainty caused by sensor and source mismatch for greater accuracy.
"Waveguide power sensors are renowned for their accuracy and low mismatch loss," said Ee Huei Sin, vice president, Agilent's General-Purpose Electronic Measurement Division. "With the E8486A, Agilent now offers a full range of waveguide power sensors to fulfill the wireless backhaul and automotive radar industries."
U.S. Pricing and Additional Information
The Agilent E8486A waveguide power sensor is now available worldwide. E8486A Option 100 (60 to 90 GHz, -30 to +20 dBm) is priced at $11,238. E8486A Option 200 (60 to 90 GHz, -60 to +20 dBm) is priced at $13,308.
Information on the E8486A is available at www.agilent.com/find/waveguidesensor_pr. High-resolution images are available at www.agilent.com/find/waveguidesensor_images.
Agilent Technologies Inc. (NYSE: A) is the world's premier measurement company and a technology leader in chemical analysis, life sciences, diagnostics, electronics and communications. The company's 20,600 employees serve customers in more than 100 countries. Agilent had revenues of $6.8 billion in fiscal 2013. Information about Agilent is available at www.agilent.com.
On Sept. 19, 2013, Agilent announced plans to separate into two publicly traded companies through a tax-free spinoff of its electronic measurement business. The new company is named Keysight Technologies, Inc. The separation is expected to be completed in early November 2014.
# # #
Contact:
Janet Smith, Americas
+1 970 679 5397
janet_smith@agilent.com
Twitter: @JSmithAgilent
Sarah Calnan, Europe
+44 (118) 927 5101
sarah_calnan@agilent.com
Iris Ng, Asia
+852 31977979
iris-hw_ng@agilent.com