Agilent Technologies Introduces Family of Basic AC Power Sources for Reliable Testing with Repeatable Results

  
  

SANTA CLARA, Calif., June 23, 2014

Agilent Technologies Inc. (NYSE: A) today introduced a family of basic AC power sources that deliver stable, reliable power for testing electronic devices during design and manufacturing. The new Agilent AC6800 Series includes four models from 500 to 4000 VA output power, all with the quality and capability required for basic testing.

For simple test applications, electronic device designers and manufacturers may need a basic AC power source to simulate outlet power or global AC power conditions. They may also need to make sure their AC-powered products operate properly when they encounter voltage fluctuations, extreme inrush current and transient spikes from today's overburdened power grid. The AC6800 Series basic power sources are ideal for powering devices under test in these situations.

The AC6800 Series basic AC power sources offer intuitive user interfaces that make it easy for engineers to access and view setup and measurement information directly from the front panel or programmatically via SCPI (Standard Commands for Programmable Instruments) commands.

The AC6800 Series sources come standard with LAN/LXI Core and USB interfaces. An optional GPIB interface is also available. The LXI Core interface enables engineers to set up and control the power supplies remotely via a standard Web interface. Users can add an optional analog input board to enable adding basic transient waveforms to their sources.

With its three-year warranty and global support from Agilent, the AC6800 Series lowers the cost of ownership and increases engineers' confidence in AC source uptime.

More information about the AC6800 Series basic power sources is available at www.agilent.com/find/AC6800. Product images are available at www.agilent.com/find/AC6800_images.

U.S. Pricing and Availability

The Agilent AC6800 basic AC power sources are available now starting at $3,498.


About Agilent Technologies

Agilent Technologies Inc. (NYSE: A) is the world's premier measurement company and a technology leader in chemical analysis, life sciences, diagnostics, electronics and communications. The company's 20,600 employees serve customers in more than 100 countries. Agilent had revenues of $6.8 billion in fiscal 2013. Information about Agilent is available at www.agilent.com.

On Sept. 19, 2013, Agilent announced plans to separate into two publicly traded companies through a tax-free spinoff of its electronic measurement business. The new company is named Keysight Technologies, Inc. The separation is expected to be completed in early November 2014.

# # #

Contact:

Janet Smith, Americas
+1 970 679 5397
[email protected]
Twitter: @JSmithAgilent

Sarah Calnan, Europe
+44 (118) 927 5101
[email protected]

Connie Wong, Asia
+852 3197-7818
[email protected]