SANTA CLARA, Calif., March 24, 2014
Agilent Technologies Inc. (NYSE: A) today introduced the industry's first LTE-A uplink 4x4 MIMO signal generation solution designed to enable R&D engineers to verify FDD and TDD LTE-A Evolved Node B receivers. The solution comprises N7624B/25B Signal Studio for LTE/LTE-Advanced FDD/TDD software with newly added support for UL 4x4 MIMO.
"Agilent, a recognized leader and provider of world-class LTE solutions, is integrally involved in the development, revision and implementation of the LTE-Advanced standard," said Jim Curran, marketing manager of Agilent's Microwave and Communications Division. "Our first-to-market UL 4x4 MIMO test solution further complements Agilent's comprehensive portfolio of LTE-Advanced signal-generation and analysis solutions, and reaffirms our commitment to leading the evolution of LTE to a 4G technology."
LTE-A is a leading fourth-generation wireless communications technology defined in Release 10, and all follow-on releases, of the 3GPP LTE standard. In Release 10, the eNB is required to support up to 8x8 MIMO in the downlink, while user equipment is required to support up to 4x4 MIMO in UL. Thanks to its recent UL 4x4 MIMO enhancement, Signal Studio is well-equipped to meet this requirement. Support for DL 8x8 MIMO was introduced last year.
In any MIMO system, ensuring the receiver correctly decodes the MIMO signal is paramount. Signal Studio with UL 4x4 MIMO support allows engineers to quickly generate a simulated 4x4 MIMO signal and download waveforms into multiple signal generators (e.g., Agilent MXG) or a baseband generator and channel emulator (e.g., Agilent PXB) for use during eNB receiver test. This capability is ideal for R&D engineers working in LTE-A early engagement, where access to real UE is generally not available. With the enhanced Signal Studio for LTE/LTE-A solution, engineers not only have a good replacement for UE at the early stage of the LTE-A standard, but also can more deeply evaluate their receivers.
Additional Signal Studio-Related Enhancements
Digital pre-distortion is a new capability being added to the LTE/LTE-A Signal Studio software. Also new is real-time LTE signal generation support for the Test Case Manager software, which works with Signal Studio.
The DPD capability works with Signal Studio's envelope tracking function to help developers test ET power amplifiers. Using the capability, developers can apply DPD to their RF and ET signals before they are fed into an ET PA or power supply.
With support for real-time LTE signal generation now available in Test Case Manager, engineers working on LTE base stations can better handle the LTE receiver conformance testing defined by 3GPP TS36.141 (including clause 7 and 8). Test Case Manager enables engineers to perform complex standard-based tests with a streamlined user interface, saving time and effort and reducing inconsistencies in procedures and test results among multiple users.
U.S. Pricing and Availability
Agilent's Signal Studio for LTE/LTE-A FDD and TDD with support for UL 4x4 MIMO, DPD and real-time LTE signal generation is now available. Pricing is as follows:
N7624/25B Signal Studio for LTE/LTE-Advanced FDD/TDD | ||
---|---|---|
Option TFP | Advanced LTE-Advanced FDD/TDD R10 | $3,339 |
Option KFP | Envelope Tracking | $1,000 |
N7649B Test Case Manager | ||
Option ETP | LTE FDD and TDD eNB receiver tests | $1,000 |
More information on Agilent's enhanced Signal Studio for LTE/LTE-Advanced is available at www.agilent.com/find/N7624B and www.agilent.com/find/N7625B. Images of the new enhancements are available at www.agilent.com/find/SignalStudioLTE_images.
Agilent Technologies Inc. (NYSE: A) is the world's premier measurement company and a technology leader in chemical analysis, life sciences, diagnostics, electronics and communications. The company's 20,600 employees serve customers in more than 100 countries. Agilent had revenues of $6.8 billion in fiscal 2013. Information about Agilent is available at www.agilent.com.
On Sept. 19, 2013, Agilent announced plans to separate into two publicly traded companies through a tax-free spinoff of its electronic measurement business. The new company is named Keysight Technologies, Inc. The separation is expected to be completed in early November 2014.
# # #
Contact:
Janet Smith, Americas
+1 970 679 5397
[email protected]
Twitter: @JSmithAgilent
Sarah Calnan, Europe
+44 (118) 927 5101
[email protected]
Connie Wong, Asia
+852 3197-7818
[email protected]