Agilent Technologies Introduces ADS DDR4 Compliance Test Bench for Solving the Simulation-Measurement Correlation Challenge

  
  

SANTA CLARA, Calif., June 30, 2014

Agilent Technologies Inc. (NYSE: A) today introduced Advanced Design System DDR4 Compliance Test Bench, which enables a complete workflow for DDR4 engineers from simulation of a candidate design through measurement of the finished prototype. The solution is ideal for semiconductor companies developing DDR controller IP; those developing DRAM chips and DIMMs; and OEMs integrating the controller and DIMM into a system using PCB technology.


The compliance test bench is available as an add-on to Advanced Design System 2014.01 software from Agilent EEsof EDA. The new test bench uses simulation to ensure that a candidate design yields a fabricated prototype compliant to the voltage and timing specifications of the JEDEC DDR4 standard. Previous tools for this task made it difficult to correlate simulation compliance with hardware prototype and test bench compliance.

The ADS DDR4 Compliance Test Bench rectifies this situation by providing a customizable test harness in which to simulate customers' intellectual property. The test bench also provides a post-processing scripting capability, known as Waveform Bridge, which exports simulated waveforms to the same compliance application used with Agilent Infiniium oscilloscopes. The new version of the Infiniium software works on live data from an oscilloscope and on stored data (offline mode). Additionally, it works on the PC embedded in the oscilloscope and on an ordinary Windows PC (remote mode). Using this new offline/remote mode, engineers can run the compliance app side-by-side with ADS.

"The new approach enabled by the offline/remote mode allows engineers to apply the same set of compliance tests in offline or remote mode," said Colin Warwick, product manager for high-speed digital design at Agilent EEsof EDA. "More importantly, engineers can now receive the same compliance report from their simulated design as they would on the fabricated prototype."

The ADS DDR4 Compliance Test Bench provides a seamless solution from simulation to hardware prototype test-all from a single company-avoiding the challenges of working with disparate solutions from different vendors.

"By leveraging our proven oscilloscope compliance application, Agilent EEsof EDA is simplifying our customers' design workflow," said Caren Johnson, high-performance oscilloscope marketing manager at Agilent. "Agilent is in the unique position of having both the industry-leading software and hardware parts of the solution in the same company, reducing the risk of relying on multiple partners."

U.S. Pricing and Availability

The DDR Compliance Test Bench will be available in August as an add-on to the presently shipping ADS 2014.01 platform. Contact your local Agilent sales office for pricing on a system specifically tailored to meet the needs of your test environment.

More information is available at www.agilent.com/find/eesof-ads-ddr4. A product image is available at www.agilent.com/find/ADSDDR4_images. A video demonstration of the ADS DDR4 Compliance Test Bench is available at http://youtu.be/x5RvmiNvGvg.

About Agilent EEsof EDA Software

Agilent EEsof EDA is the leading supplier of electronic design automation software for microwave, RF, high-frequency, high-speed digital, RF system, electronic system level, circuit, 3-D electromagnetic, physical design and device-modeling applications. More information is available at www.agilent.com/find/eesof.


About Agilent Technologies

Agilent Technologies Inc. (NYSE: A) is the world's premier measurement company and a technology leader in chemical analysis, life sciences, diagnostics, electronics and communications. The company's 20,600 employees serve customers in more than 100 countries. Agilent had revenues of $6.8 billion in fiscal 2013. Information about Agilent is available at www.agilent.com.

On Sept. 19, 2013, Agilent announced plans to separate into two publicly traded companies through a tax-free spinoff of its electronic measurement business. The new company is named Keysight Technologies, Inc. The separation is expected to be completed in early November 2014.

# # #

Contact:

Janet Smith, Americas
+1 970 679 5397
[email protected]
Twitter: @JSmithAgilent

Sarah Calnan, Europe
+44 (118) 927 5101
[email protected]

Connie Wong, Asia
+852 3197-7818
[email protected]